<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPF0100 Default configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-Default-configuration/m-p/644481#M98351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. In default mode of PF0100 there is no mention about the following supplies:&lt;/P&gt;&lt;P&gt;SWBST_VOLT,&amp;nbsp;VGEN1_VOLT and&amp;nbsp;VGEN3_VOLT. Does it mean that these supplies are not enabled?&lt;/P&gt;&lt;P&gt;2. Default configuration of register SWBSTCTL as per data sheet says the SWBST_VOLT is configured as 'ON' and configured for 5.0V.&lt;/P&gt;&lt;P&gt;3. For LDO's there are 4&amp;nbsp;bits (3:0) for output setting marked as VGENx (Register VGENxCTL) and its default value is mentioned as 0x80. The maximum value 4 bits can achieve is 0x0F. Is this a typing mistake?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer the attachment below for more details.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Apr 2017 02:59:40 GMT</pubDate>
    <dc:creator>abhijit_mote</dc:creator>
    <dc:date>2017-04-27T02:59:40Z</dc:date>
    <item>
      <title>PF0100 Default configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-Default-configuration/m-p/644481#M98351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. In default mode of PF0100 there is no mention about the following supplies:&lt;/P&gt;&lt;P&gt;SWBST_VOLT,&amp;nbsp;VGEN1_VOLT and&amp;nbsp;VGEN3_VOLT. Does it mean that these supplies are not enabled?&lt;/P&gt;&lt;P&gt;2. Default configuration of register SWBSTCTL as per data sheet says the SWBST_VOLT is configured as 'ON' and configured for 5.0V.&lt;/P&gt;&lt;P&gt;3. For LDO's there are 4&amp;nbsp;bits (3:0) for output setting marked as VGENx (Register VGENxCTL) and its default value is mentioned as 0x80. The maximum value 4 bits can achieve is 0x0F. Is this a typing mistake?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer the attachment below for more details.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 02:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-Default-configuration/m-p/644481#M98351</guid>
      <dc:creator>abhijit_mote</dc:creator>
      <dc:date>2017-04-27T02:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 Default configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-Default-configuration/m-p/644482#M98352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. The SWBST, VGEN1 and VGEN3 supplies are by default Off in the Default power-on configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. There is no single reset configuration for supply control registers, it depends on the power-on configuration selected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. This is just a typo. Of course, the value of 0x8 is meant.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Apr 2017 08:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-Default-configuration/m-p/644482#M98352</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-04-30T08:41:59Z</dc:date>
    </item>
  </channel>
</rss>