<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RAM Memory usage measurement tool for iMX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Memory-usage-measurement-tool-for-iMX6Q/m-p/644389#M98343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I'm using iMX6Q processor with the BSP provided and developed many application in c/c++. Now i want measure the usage of RAM by each application with modules wise not just USS or PSS and also need to detect memory leaks at run time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me some tool with document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Thiru N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Dec 2016 08:32:31 GMT</pubDate>
    <dc:creator>nthiru28</dc:creator>
    <dc:date>2016-12-28T08:32:31Z</dc:date>
    <item>
      <title>RAM Memory usage measurement tool for iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Memory-usage-measurement-tool-for-iMX6Q/m-p/644389#M98343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I'm using iMX6Q processor with the BSP provided and developed many application in c/c++. Now i want measure the usage of RAM by each application with modules wise not just USS or PSS and also need to detect memory leaks at run time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me some tool with document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Thiru N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 08:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-Memory-usage-measurement-tool-for-iMX6Q/m-p/644389#M98343</guid>
      <dc:creator>nthiru28</dc:creator>
      <dc:date>2016-12-28T08:32:31Z</dc:date>
    </item>
    <item>
      <title>Re: RAM Memory usage measurement tool for iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Memory-usage-measurement-tool-for-iMX6Q/m-p/644390#M98344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First, you can use some generic debug tools, such as GDB/KGDB. Please refer to the following Application Note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, please just search the internet, there are many open source monitoring/debugging tools for Linux. For example, look here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.tecmint.com%2Fcommand-line-tools-to-monitor-linux-performance%2F" rel="nofollow" target="_blank"&gt;http://www.tecmint.com/command-line-tools-to-monitor-linux-performance/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 12:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-Memory-usage-measurement-tool-for-iMX6Q/m-p/644390#M98344</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-01-09T12:03:42Z</dc:date>
    </item>
  </channel>
</rss>