<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6qp probably damaged</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-probably-damaged/m-p/644237#M98321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did several measurements and soldering/desoldering on a custom boards, experiencing now imxq6p that goes very hot in abt 5 seconds at boot, so it looks to me as damaged. Luckily i have multiple boards, but it's the first time it's happen. Could the imx6qp be damaged ? If yes, as it seems, what could be possible causes ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Feb 2017 16:01:03 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2017-02-16T16:01:03Z</dc:date>
    <item>
      <title>imx6qp probably damaged</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-probably-damaged/m-p/644237#M98321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did several measurements and soldering/desoldering on a custom boards, experiencing now imxq6p that goes very hot in abt 5 seconds at boot, so it looks to me as damaged. Luckily i have multiple boards, but it's the first time it's happen. Could the imx6qp be damaged ? If yes, as it seems, what could be possible causes ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 16:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-probably-damaged/m-p/644237#M98321</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2017-02-16T16:01:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx6qp probably damaged</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6qp-probably-damaged/m-p/644238#M98322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Angelo Dureghello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Excessive manipulation may indeed damage the chip package, which is true for any component. Most i.MX6 part numbers withstand tree reflow cycles provided that the JEDEC standards are followed. You may find more information regarding the soldering limits on AN3298 (link below).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3298.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3298.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other kind of damages may also occur like ESD damage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 21:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6qp-probably-damaged/m-p/644238#M98322</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-02-16T21:13:29Z</dc:date>
    </item>
  </channel>
</rss>