<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEnabling Central Security Unit on IMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Central-Security-Unit-on-IMX6/m-p/643997#M98294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm testing OP-TEE on the IMX6 Sabre SD board and my objective is to setup a UART communication between the TEE and an external device. I successfully enabled the UART and I'm able to establish the serial link, but in order to increase the security level, I would like to manage the CSU, so the UART (UART4 in my case) will only be available for secure world and not for normal world (a Linux Yocto-based config). If I set CSL35[23:16] to 0xFF, everything works. If I set CSL35[23:16] to 0x33, I have a core data-abort error as soon as the TEE tries to write on the UART. The fault seems to be a asynchronous external abort... Does anyone already succeed to enable the CSU on IMX6 ? I don't really understand the role of the HP Register field. Maybe the TZASC (Trust Zone Address Space Config) must be initialized first ? Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Mar 2017 09:56:33 GMT</pubDate>
    <dc:creator>ogfr</dc:creator>
    <dc:date>2017-03-13T09:56:33Z</dc:date>
    <item>
      <title>Enabling Central Security Unit on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Central-Security-Unit-on-IMX6/m-p/643997#M98294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm testing OP-TEE on the IMX6 Sabre SD board and my objective is to setup a UART communication between the TEE and an external device. I successfully enabled the UART and I'm able to establish the serial link, but in order to increase the security level, I would like to manage the CSU, so the UART (UART4 in my case) will only be available for secure world and not for normal world (a Linux Yocto-based config). If I set CSL35[23:16] to 0xFF, everything works. If I set CSL35[23:16] to 0x33, I have a core data-abort error as soon as the TEE tries to write on the UART. The fault seems to be a asynchronous external abort... Does anyone already succeed to enable the CSU on IMX6 ? I don't really understand the role of the HP Register field. Maybe the TZASC (Trust Zone Address Space Config) must be initialized first ? Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 09:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Central-Security-Unit-on-IMX6/m-p/643997#M98294</guid>
      <dc:creator>ogfr</dc:creator>
      <dc:date>2017-03-13T09:56:33Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling Central Security Unit on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Central-Security-Unit-on-IMX6/m-p/643998#M98295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olivier&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately there is no support for TEE in nxp bsps, however it can be supported using&lt;/P&gt;&lt;P&gt;&amp;nbsp;Professional Services:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fsupport%2Fnxp-professional-services%3APROFESSIONAL-SERVICE" rel="nofollow" target="_blank"&gt;http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 23:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Central-Security-Unit-on-IMX6/m-p/643998#M98295</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-13T23:18:56Z</dc:date>
    </item>
  </channel>
</rss>