<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCouldn't automate eMMC booting using MFG tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Couldn-t-automate-eMMC-booting-using-MFG-tool/m-p/643938#M98282</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using IMX6DL based custom board.&lt;/P&gt;&lt;P&gt;I am trying to boot from eMMC, and I am able to do so, but only after manually setting boot_config.&lt;/P&gt;&lt;P&gt;It seems like this line from MFG tool doesn't work. I can not find the reason.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="$ echo 8 &amp;gt; /sys/block/mmcblk%mmc%/device/boot_config"&amp;gt;enable boot partion 1 to boot&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried with this lines also, since I was able to find boot_config there too. Again unsuccessfully.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="$ echo 8 &amp;gt; /sys/devices/soc0/soc.1/2100000.aips-bus/219c000.usdhc/mmc_host/mmc0/mmc0\:0001/boot_config"&amp;gt;enable boot partion 1 to boot&amp;lt;/CMD&amp;gt;&lt;BR /&gt; &amp;lt;CMD state="Updater" type="push" body="$ echo 10 &amp;gt; /sys/devices/soc0/soc.1/2100000.aips-bus/219c000.usdhc/mmc_host/mmc0/mmc0\:0001/boot_bus_config"&amp;gt;enable boot partion 1 to boot&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I set up this manually(after starting u-boot.imx and kernel directly from RAM using MFG tool) I can see bit for boot enabling set to 1, and after repower the board, it does boots up from eMMC fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what could be the problem with MFG tool command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Feb 2017 17:19:28 GMT</pubDate>
    <dc:creator>bazo00</dc:creator>
    <dc:date>2017-02-16T17:19:28Z</dc:date>
    <item>
      <title>Couldn't automate eMMC booting using MFG tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Couldn-t-automate-eMMC-booting-using-MFG-tool/m-p/643938#M98282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using IMX6DL based custom board.&lt;/P&gt;&lt;P&gt;I am trying to boot from eMMC, and I am able to do so, but only after manually setting boot_config.&lt;/P&gt;&lt;P&gt;It seems like this line from MFG tool doesn't work. I can not find the reason.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="$ echo 8 &amp;gt; /sys/block/mmcblk%mmc%/device/boot_config"&amp;gt;enable boot partion 1 to boot&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried with this lines also, since I was able to find boot_config there too. Again unsuccessfully.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="$ echo 8 &amp;gt; /sys/devices/soc0/soc.1/2100000.aips-bus/219c000.usdhc/mmc_host/mmc0/mmc0\:0001/boot_config"&amp;gt;enable boot partion 1 to boot&amp;lt;/CMD&amp;gt;&lt;BR /&gt; &amp;lt;CMD state="Updater" type="push" body="$ echo 10 &amp;gt; /sys/devices/soc0/soc.1/2100000.aips-bus/219c000.usdhc/mmc_host/mmc0/mmc0\:0001/boot_bus_config"&amp;gt;enable boot partion 1 to boot&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I set up this manually(after starting u-boot.imx and kernel directly from RAM using MFG tool) I can see bit for boot enabling set to 1, and after repower the board, it does boots up from eMMC fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what could be the problem with MFG tool command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 17:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Couldn-t-automate-eMMC-booting-using-MFG-tool/m-p/643938#M98282</guid>
      <dc:creator>bazo00</dc:creator>
      <dc:date>2017-02-16T17:19:28Z</dc:date>
    </item>
    <item>
      <title>Re: Couldn't automate eMMC booting using MFG tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Couldn-t-automate-eMMC-booting-using-MFG-tool/m-p/643939#M98283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if appropriate version of MFG Tools used, for example&lt;/P&gt;&lt;P&gt;for L4.1.15_1.1.0 should be used i.MX Series Manufacturing Toolkit for Linux 4.1.15_1.1.0 Release , e.t.c.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;What nxp reference design is based custom board, sould it be reproduced on reference board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 23:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Couldn-t-automate-eMMC-booting-using-MFG-tool/m-p/643939#M98283</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-16T23:31:17Z</dc:date>
    </item>
  </channel>
</rss>