<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Software Uart Using GPIO's. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Software-Uart-Using-GPIO-s/m-p/643348#M98226</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vipul Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a simple buy excellent tutorial on how to setup a simple Device Tree on the following document. You may find it useful as the first step would be setting the GPIOs on your Device Tree (which is introduced starting Kernel 3.10)&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-329664"&gt;https://community.nxp.com/docs/DOC-329664&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are also examples of a GPIO device tree in the communities, as for example the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/519839"&gt;https://community.nxp.com/message/519839&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the actual UART Software implementation there is not an App Note covering this but you may find some software UART examples on the web. It may not be as straightforward as it sounds but already available open source software may help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Oct 2016 17:05:03 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-10-18T17:05:03Z</dc:date>
    <item>
      <title>Software Uart Using GPIO's.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Software-Uart-Using-GPIO-s/m-p/643347#M98225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a customised i.MX6 Dual board. The board supports 4 UART's but all are used. So, I need to use software UART. I am having 2 GPIO's that I need to configure as UART's Rx and Tx.&lt;/P&gt;&lt;P&gt;OS - Linux&lt;/P&gt;&lt;P&gt;Kernel - 3.10&lt;/P&gt;&lt;P&gt;BSP - Yocto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody suggest me how to configure GPIO's as a UART or refer some code example ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 05:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Software-Uart-Using-GPIO-s/m-p/643347#M98225</guid>
      <dc:creator>vipulkumar</dc:creator>
      <dc:date>2016-10-18T05:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Software Uart Using GPIO's.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Software-Uart-Using-GPIO-s/m-p/643348#M98226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vipul Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a simple buy excellent tutorial on how to setup a simple Device Tree on the following document. You may find it useful as the first step would be setting the GPIOs on your Device Tree (which is introduced starting Kernel 3.10)&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-329664"&gt;https://community.nxp.com/docs/DOC-329664&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are also examples of a GPIO device tree in the communities, as for example the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/519839"&gt;https://community.nxp.com/message/519839&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the actual UART Software implementation there is not an App Note covering this but you may find some software UART examples on the web. It may not be as straightforward as it sounds but already available open source software may help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 17:05:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Software-Uart-Using-GPIO-s/m-p/643348#M98226</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-10-18T17:05:03Z</dc:date>
    </item>
  </channel>
</rss>