<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NAND boot problem after enable SECURE_BOOT in uboot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NAND-boot-problem-after-enable-SECURE-BOOT-in-uboot/m-p/643304#M98210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following may help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/380130"&gt;https://community.nxp.com/thread/380130&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2016 09:21:27 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-09-26T09:21:27Z</dc:date>
    <item>
      <title>NAND boot problem after enable SECURE_BOOT in uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-boot-problem-after-enable-SECURE-BOOT-in-uboot/m-p/643303#M98209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using IMX6UL EVK with IMX6UL chip in open mode I can boot from NAND without any problem&lt;/P&gt;&lt;P&gt;but only if CONFIG_SECURE_BOOT is not enabled in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if enable CONFIG_SECURE_BOOT in uboot then booting from NAND no longer works,&lt;/P&gt;&lt;P&gt;I get no output. (Device is in open mode so booting should work even if image is not signed ...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This same uboot image (with CONFIG_SECURE_BOOT) boots just fine when loaded via USB ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have also tried burning the signed uboot image to NAND and still nothing on the output.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 19:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-boot-problem-after-enable-SECURE-BOOT-in-uboot/m-p/643303#M98209</guid>
      <dc:creator>SJA</dc:creator>
      <dc:date>2016-09-22T19:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: NAND boot problem after enable SECURE_BOOT in uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-boot-problem-after-enable-SECURE-BOOT-in-uboot/m-p/643304#M98210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following may help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/380130"&gt;https://community.nxp.com/thread/380130&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 09:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-boot-problem-after-enable-SECURE-BOOT-in-uboot/m-p/643304#M98210</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-26T09:21:27Z</dc:date>
    </item>
  </channel>
</rss>