<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR Consumption in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Consumption/m-p/643189#M98182</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eli Az,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no much information available but perhaps Application Note 4580 (link below) may be of help. There are some charts in which the different modules are managed separately for power measurement. Please note that it would also depend on the memory used etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/files/32bit/doc/app_note/AN4580.pdf" title="http://www.nxp.com/files/32bit/doc/app_note/AN4580.pdf"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN4580.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 20:48:04 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-09-22T20:48:04Z</dc:date>
    <item>
      <title>DDR Consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Consumption/m-p/643188#M98181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where can I find specs about NVCC_DRAM consumption(for LPDDR2 )?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 11:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Consumption/m-p/643188#M98181</guid>
      <dc:creator>eliaz</dc:creator>
      <dc:date>2016-09-22T11:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Consumption/m-p/643189#M98182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eli Az,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no much information available but perhaps Application Note 4580 (link below) may be of help. There are some charts in which the different modules are managed separately for power measurement. Please note that it would also depend on the memory used etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/files/32bit/doc/app_note/AN4580.pdf" title="http://www.nxp.com/files/32bit/doc/app_note/AN4580.pdf"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN4580.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 20:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Consumption/m-p/643189#M98182</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-09-22T20:48:04Z</dc:date>
    </item>
  </channel>
</rss>