<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Xfbdev with mouse and tslib is not working simultaneously</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xfbdev-with-mouse-and-tslib-is-not-working-simultaneously/m-p/191690#M9811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe it is a bit outdated, but still there's the answer:&lt;/P&gt;&lt;P&gt;Xfbdev :0 -screen 480x800 -mouse tslib,1,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice &amp;amp;&lt;/P&gt;&lt;P&gt;It is working imx.51 with USB mouse and touchscreen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Apr 2012 09:08:34 GMT</pubDate>
    <dc:creator>MaciejSuminski</dc:creator>
    <dc:date>2012-04-17T09:08:34Z</dc:date>
    <item>
      <title>Xfbdev with mouse and tslib is not working simultaneously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xfbdev-with-mouse-and-tslib-is-not-working-simultaneously/m-p/191689#M9810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am working on the board i.mx53 SMD tablet, booted with 11.05 build&lt;BR /&gt;images.&lt;BR /&gt;&lt;BR /&gt;Touch pad with Xfbdev is working fine with the below Xfbdev command.&lt;BR /&gt;&lt;BR /&gt;Xfbdev -screen 1024x768 -mouse tslib,,device=/dev/input/ts0&amp;nbsp; &amp;amp;&lt;BR /&gt;&lt;BR /&gt;When I use with -mouse option (as given below) to work mouse simultaneously with the touch screen,&lt;BR /&gt;touch screen is not working properly. Means, &lt;BR /&gt;for the contact on touchpad - the cursor points to wrong coordinates.&lt;BR /&gt;and for the release of contact - the cursor came to right coordinate (where the contact happened).&lt;BR /&gt;&lt;BR /&gt;Xfbdev -mouse tslib,,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&amp;amp;&lt;BR /&gt;&lt;BR /&gt;When I use the mouse, its changing to mouse protocol, as shown in below message.&lt;BR /&gt;&lt;BR /&gt;Switching to mouse protocol "imps/2"&lt;BR /&gt;Switching to mouse protocol "exps/2"&lt;BR /&gt;Switching to mouse protocol "bus"&lt;BR /&gt;Switching to mouse protocol "ps/2"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;After this, once I do ts_calibrate again, the touch is working fine.&lt;BR /&gt;&lt;BR /&gt;Is it possible to use touch and mouse simultaneously with Xfbdev server ?&lt;BR /&gt;&lt;BR /&gt;Please suggest me in a way forward.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Nagesh A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2011 06:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xfbdev-with-mouse-and-tslib-is-not-working-simultaneously/m-p/191689#M9810</guid>
      <dc:creator>nagesha71</dc:creator>
      <dc:date>2011-11-29T06:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: Xfbdev with mouse and tslib is not working simultaneously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xfbdev-with-mouse-and-tslib-is-not-working-simultaneously/m-p/191690#M9811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe it is a bit outdated, but still there's the answer:&lt;/P&gt;&lt;P&gt;Xfbdev :0 -screen 480x800 -mouse tslib,1,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice &amp;amp;&lt;/P&gt;&lt;P&gt;It is working imx.51 with USB mouse and touchscreen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Apr 2012 09:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xfbdev-with-mouse-and-tslib-is-not-working-simultaneously/m-p/191690#M9811</guid>
      <dc:creator>MaciejSuminski</dc:creator>
      <dc:date>2012-04-17T09:08:34Z</dc:date>
    </item>
  </channel>
</rss>