<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: blown efuse via uart in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/blown-efuse-via-uart/m-p/191678#M9809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sergey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are looking the procedure to blow the eFUSE values to boot from SATA interface for IMX6 based device. did you find the procedure to blow the eFUSE using UART or USB interface or is there any tool to do the same.?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jan 2013 23:10:02 GMT</pubDate>
    <dc:creator>ManoharChinnadu</dc:creator>
    <dc:date>2013-01-08T23:10:02Z</dc:date>
    <item>
      <title>blown efuse via uart</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/blown-efuse-via-uart/m-p/191677#M9808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I have problem.&lt;/P&gt;&lt;P&gt;I have custom board with iMX537 processor. In project I haven't placed switch to configurate processor via GPIO (set eFUSE via GPIO).&lt;/P&gt;&lt;P&gt;I reference manual I've found serial protocol description to configurate processor via uart. Also, there says what via uart user can programm eFUSE. But I can't do that. For example, I send next command via uart&lt;/P&gt;&lt;P&gt;02 02 00 00 08 14 08 00 00 00 00 00 00 00 19 00&lt;/P&gt;&lt;P&gt;This command is for configurate CFG3[7:0] eFUSE&lt;/P&gt;&lt;P&gt;I receive ack&lt;/P&gt;&lt;P&gt;56 78 78 56&lt;/P&gt;&lt;P&gt;After that I send next command&lt;/P&gt;&lt;P&gt;01 01 00 00 08 14 08 00 00 00 01 00 00 00 00 00&lt;/P&gt;&lt;P&gt;And receive ack&lt;/P&gt;&lt;P&gt;56 78 78 56 02&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I wrote 0x19 and I've read 0x02.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In reference manual says, what 0x00 00 08 14 is the addrress for CFG3[7:0] eFUSE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody help me to undestand how can I programm eFuse via uart.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2012 03:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/blown-efuse-via-uart/m-p/191677#M9808</guid>
      <dc:creator>ciberbob</dc:creator>
      <dc:date>2012-09-13T03:50:27Z</dc:date>
    </item>
    <item>
      <title>Re: blown efuse via uart</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/blown-efuse-via-uart/m-p/191678#M9809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sergey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are looking the procedure to blow the eFUSE values to boot from SATA interface for IMX6 based device. did you find the procedure to blow the eFUSE using UART or USB interface or is there any tool to do the same.?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2013 23:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/blown-efuse-via-uart/m-p/191678#M9809</guid>
      <dc:creator>ManoharChinnadu</dc:creator>
      <dc:date>2013-01-08T23:10:02Z</dc:date>
    </item>
  </channel>
</rss>