<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: More SATA boot questions</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/More-SATA-boot-questions/m-p/191636#M9802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Do you solved the question?&lt;/P&gt;&lt;P&gt;I meet the same problem as you. When I sata info, I get as follows:&lt;/P&gt;&lt;P&gt;&lt;I&gt;MX53-ARD-DDR3 U-Boot &amp;gt; sata info&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;flags: ncq stag pm led clo only pmp pio slum part&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;timeout exit!&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;timeout exit!&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;SATA Device Info:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;S/N:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;Product model number:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;Firmware version:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;Capacity: 0 sectors&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&amp;nbsp;&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;SATA device 0: Model:&amp;nbsp; Firm:&amp;nbsp; Ser#:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Hard Disk&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: not available&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks different with your result such as I cannot get the SATA's capacity but you can. Why SATA device cannot be recognized?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Feb 2012 08:14:57 GMT</pubDate>
    <dc:creator>peterliu1</dc:creator>
    <dc:date>2012-02-29T08:14:57Z</dc:date>
    <item>
      <title>More SATA boot questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-SATA-boot-questions/m-p/191635#M9801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I reviewed the discussion at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://imxcommunity.org/group/imx53quickstartboard/forum/topics/how-to-prepare-sata-disk-for?commentId=4103961%3AComment%3A14843&amp;amp;groupId=4103961%3AGroup%3A5816"&gt;http://imxcommunity.org/group/imx53quickstartboard/forum/topics/how-to-prepare-sata-disk-for?commentId=4103961%3AComment%3A14843&amp;amp;groupId=4103961%3AGroup%3A5816&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Then set out to try this but I can not seem to get the QSB the default Ubuntu Image from a ﻿SATA hard disk drive.&lt;/P&gt;&lt;P&gt;I am sure I missing some obvious step like how does uBoot get onto the hard drive.&amp;nbsp; The uImage file I am working with is uImage-744-g27fdf7b taken directly from the /boot directory from the QSB.&lt;/P&gt;&lt;P&gt;I documented the procedure that I have followed in some detail below:&lt;BR /&gt;Any help from someone who has this working would be much appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Steps taken so far:&lt;/P&gt;&lt;P&gt;0. Verified 2.1 version silicon&lt;/P&gt;&lt;P&gt;1. Copy the ﻿uImage-744-g27fdf7b to my PC TFTP server home directory&lt;/P&gt;&lt;P&gt;2. Rename the file to uImage&lt;/P&gt;&lt;P&gt;3. Soldered on a dip switch onto SW1&lt;/P&gt;&lt;P&gt;4. Changed R46 from a pull-up to a pull-down (the board no longer booted uBoot once I changed R46 to pull-down I so I added an external switch to set R46 as either pull-up or pull-down as needed)&lt;/P&gt;&lt;P&gt;5. Reset R46 to pull-up.&lt;BR /&gt;Set all SW1 dip switches off&lt;BR /&gt;(Should be QSB default configuration)&lt;/P&gt;&lt;P&gt;6. Executed uBoot commands from section 6.2 and repeated in 8.3 i.MX53 Start Linux User's Guide)&lt;/P&gt;&lt;P&gt;﻿﻿setenv serverip 192.168.180.89&lt;BR /&gt;setenv bootfile uImage&lt;BR /&gt;saveenv&lt;BR /&gt;dhcp&lt;BR /&gt;sata info&lt;BR /&gt;sata write ${loadaddr} 0x800 0x2000&lt;BR /&gt;setenv bootargs_sata 'setenv bootargs ${bootargs} console=tty1 root=/dev/sda1 ﻿﻿rootwait rw video=mxcdi1fb:BGR24,XGA di1_primary tve'&lt;BR /&gt;setenv bootcmd_sata 'run bootargs_base bootargs_sata; sata read ${loadaddr} 0x800 0x2000; bootm'&lt;BR /&gt;setenv bootcmd 'run bootcmd_sata'&lt;BR /&gt;saveenv&lt;BR /&gt;reset&lt;/P&gt;&lt;P&gt;uboot session output&lt;BR /&gt;-------------------&lt;/P&gt;&lt;P&gt;U-Boot 2009.08 (Mar 23 2011 - 12:37:03)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX53 family 2.1V at 1000 MHz&lt;BR /&gt;mx53 pll1: 1000MHz&lt;BR /&gt;mx53 pll2: 400MHz&lt;BR /&gt;mx53 pll3: 216MHz&lt;BR /&gt;mx53 pll4: 455MHz&lt;BR /&gt;ipg clock : 66666666Hz&lt;BR /&gt;ipg per clock : 33333333Hz&lt;BR /&gt;uart clock : 21600000Hz&lt;BR /&gt;cspi clock : 54000000Hz&lt;BR /&gt;ahb clock : 133333333Hz&lt;BR /&gt;axi_a clock : 400000000Hz&lt;BR /&gt;axi_b clock : 200000000Hz&lt;BR /&gt;emi_slow clock: 133333333Hz&lt;BR /&gt;ddr clock : 400000000Hz&lt;BR /&gt;esdhc1 clock : 80000000Hz&lt;BR /&gt;esdhc2 clock : 80000000Hz&lt;BR /&gt;esdhc3 clock : 80000000Hz&lt;BR /&gt;esdhc4 clock : 80000000Hz&lt;BR /&gt;nfc clock : 26666666Hz&lt;BR /&gt;Board: MX53-LOCO 1.0&lt;BR /&gt;Boot Reason: [POR]&lt;BR /&gt;Boot Device: SD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GB&lt;BR /&gt;MMC: FSL_ESDHC: 0, FSL_ESDHC: 1&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: got MAC address from IIM: 00:04:9f:01:e1:9f&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; setenv serverip 192.168.180.89&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; setenv bootfile uImage&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; saveenv&lt;BR /&gt;Saving Environment to MMC...&lt;BR /&gt;Writing to MMC(0)... done&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; dhcp&lt;BR /&gt;FEC: enable RMII gasket&lt;BR /&gt;PHY indentify @ 0x0 = 0x0007c0f1&lt;BR /&gt;BOOTP broadcast 1&lt;BR /&gt;FEC: Link is down 7809&lt;BR /&gt;BOOTP broadcast 2&lt;BR /&gt;DHCP client bound to address 192.168.180.125&lt;BR /&gt;Using FEC0 device&lt;BR /&gt;TFTP from server 192.168.180.89; our IP address is 192.168.180.125&lt;BR /&gt;Filename 'uImage'.&lt;BR /&gt;Load address: 0x70800000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;############################################################&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 2967484 (2d47bc hex)&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; sata info&lt;BR /&gt;AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;BR /&gt;flags: ncq stag pm led clo only pmp pio slum part&lt;BR /&gt;SATA Device Info:&lt;BR /&gt;S/N:&lt;BR /&gt;Product model number:&lt;BR /&gt;Firmware version:&lt;BR /&gt;Capacity: 625142448 sectors&lt;/P&gt;&lt;P&gt;SATA device 0: Model: Firm: Ser#:&lt;BR /&gt;Type: Hard Disk&lt;BR /&gt;Supports 48-bit addressing&lt;BR /&gt;Capacity: 305245.3 MB = 298.0 GB (625142448 x 512)&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; sata write ${loadaddr} 0x800 0x2000&lt;/P&gt;&lt;P&gt;SATA write: device 0 block # 2048, count 8192 ... 8192 blocks written: OK&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; setenv bootargs_sata 'setenv bootargs ${bootargs} console=tty1 root=/dev/sda1 rootwait rw video=mxcdi1fb:BGR24,XGA di1_primary tve'&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; setenv bootcmd_sata 'run bootargs_base bootargs_sata; sata read ${loadaddr} 0x800 0x2000; bootm'&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; setenv bootcmd 'run bootcmd_sata'&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; saveenv&lt;BR /&gt;Saving Environment to MMC...&lt;BR /&gt;Writing to MMC(0)... done&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt;&lt;/P&gt;&lt;P&gt;--------------&lt;/P&gt;&lt;P&gt;7. ﻿ According to HW reference manual (pp 46,60)&lt;/P&gt;&lt;P&gt;Set Boot Switch (SW1) - Switch 6 On (shorts pin 6 to pin 15)&lt;BR /&gt;- Switch 8 On (shorts pin 8 to pin 13)&lt;BR /&gt;Set R46 to pull-down&lt;/P&gt;&lt;P&gt;8. Reset the QSB&lt;/P&gt;&lt;P&gt;No response on the serial port.&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------&lt;/P&gt;&lt;P&gt;There are several questions I have after reading the docs:&lt;/P&gt;&lt;P&gt;What is in uImage (does it include uBoot? does it include rootfs or just the kernel proper?)&lt;/P&gt;&lt;P&gt;Does the SATA drive need to be partioned or pre-formatted before uImage is loaded?&lt;/P&gt;&lt;P&gt;Does rootfs need to be copied over to the drive first (It was not clear to me if instructions section 7 in the Linux Start User Guide apply or are an alternative load procedure)&lt;/P&gt;&lt;P&gt;Lastly, are there any Linux kernel configuration file sthat need to be modified (ie fstab, grub.conf ....)?&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Mich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2011 21:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-SATA-boot-questions/m-p/191635#M9801</guid>
      <dc:creator>JeffMichalski</dc:creator>
      <dc:date>2011-11-28T21:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: More SATA boot questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-SATA-boot-questions/m-p/191636#M9802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Do you solved the question?&lt;/P&gt;&lt;P&gt;I meet the same problem as you. When I sata info, I get as follows:&lt;/P&gt;&lt;P&gt;&lt;I&gt;MX53-ARD-DDR3 U-Boot &amp;gt; sata info&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;flags: ncq stag pm led clo only pmp pio slum part&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;timeout exit!&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;timeout exit!&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;SATA Device Info:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;S/N:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;Product model number:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;Firmware version:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;Capacity: 0 sectors&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&amp;nbsp;&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;SATA device 0: Model:&amp;nbsp; Firm:&amp;nbsp; Ser#:&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Hard Disk&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&lt;I&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: not available&lt;/I&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks different with your result such as I cannot get the SATA's capacity but you can. Why SATA device cannot be recognized?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Feb 2012 08:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-SATA-boot-questions/m-p/191636#M9802</guid>
      <dc:creator>peterliu1</dc:creator>
      <dc:date>2012-02-29T08:14:57Z</dc:date>
    </item>
  </channel>
</rss>