<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX7 ADC VREF</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-ADC-VREF/m-p/642087#M98004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to figure out what the VREF for the ADCs is. It is mentioned in table 89 in the datasheet for specifying the input voltage but I can't find the specification for VREF itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also looking for some specification from which I can calculate my maximum input impedance. This must have something to do with sample rate etc. as this is ultimately and RC coupling that needs to be charged/discharged. I only intend to measure dc-voltages.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Apr 2017 07:40:58 GMT</pubDate>
    <dc:creator>thomaskofoedhan</dc:creator>
    <dc:date>2017-04-03T07:40:58Z</dc:date>
    <item>
      <title>IMX7 ADC VREF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-ADC-VREF/m-p/642087#M98004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to figure out what the VREF for the ADCs is. It is mentioned in table 89 in the datasheet for specifying the input voltage but I can't find the specification for VREF itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also looking for some specification from which I can calculate my maximum input impedance. This must have something to do with sample rate etc. as this is ultimately and RC coupling that needs to be charged/discharged. I only intend to measure dc-voltages.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 07:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-ADC-VREF/m-p/642087#M98004</guid>
      <dc:creator>thomaskofoedhan</dc:creator>
      <dc:date>2017-04-03T07:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7 ADC VREF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-ADC-VREF/m-p/642088#M98005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The ADC VREF relates to VDDA_ADC1_1P8 and VDDA_ADC2_1P8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 08:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-ADC-VREF/m-p/642088#M98005</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-04-03T08:12:51Z</dc:date>
    </item>
  </channel>
</rss>