<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Creating an extra framebuffer for imx6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Creating-an-extra-framebuffer-for-imx6UL/m-p/641817#M97969</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Is it possible to create an extra framebuffer for imx6UL. I need two framebuffers (/dev/fb0 and /dev/fb1) to be associate with the LCDIF interface of imx6UL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 10:13:31 GMT</pubDate>
    <dc:creator>zc_tee</dc:creator>
    <dc:date>2016-09-22T10:13:31Z</dc:date>
    <item>
      <title>Creating an extra framebuffer for imx6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-an-extra-framebuffer-for-imx6UL/m-p/641817#M97969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Is it possible to create an extra framebuffer for imx6UL. I need two framebuffers (/dev/fb0 and /dev/fb1) to be associate with the LCDIF interface of imx6UL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 10:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-an-extra-framebuffer-for-imx6UL/m-p/641817#M97969</guid>
      <dc:creator>zc_tee</dc:creator>
      <dc:date>2016-09-22T10:13:31Z</dc:date>
    </item>
    <item>
      <title>Re: Creating an extra framebuffer for imx6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-an-extra-framebuffer-for-imx6UL/m-p/641818#M97970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check linux documentation related to framebuffer&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.tldp.org/HOWTO/text/Framebuffer-HOWTO" title="http://www.tldp.org/HOWTO/text/Framebuffer-HOWTO"&gt;http://www.tldp.org/HOWTO/text/Framebuffer-HOWTO&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://unix.stackexchange.com/questions/98389/how-can-i-add-an-additional-framebuffer-device-in-linux" title="http://unix.stackexchange.com/questions/98389/how-can-i-add-an-additional-framebuffer-device-in-linux"&gt;How can I add an additional framebuffer device in Linux? - Unix &amp;amp; Linux Stack Exchange&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 23:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-an-extra-framebuffer-for-imx6UL/m-p/641818#M97970</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-23T23:40:58Z</dc:date>
    </item>
  </channel>
</rss>