<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Sabre_lite SD3 Card Detect Pin (GPIO) debounce in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-lite-SD3-Card-Detect-Pin-GPIO-debounce/m-p/641432#M97912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hamza&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid i.MX6 GPIOs does not have hardware debounce support.&lt;/P&gt;&lt;P&gt;One can look at pin description on AN5078 Influence of Pin Setting on System Function and Performance&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf" title="http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 02 Apr 2017 23:23:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-02T23:23:24Z</dc:date>
    <item>
      <title>Sabre_lite SD3 Card Detect Pin (GPIO) debounce</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-lite-SD3-Card-Detect-Pin-GPIO-debounce/m-p/641431#M97911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using sabre_lite target (IMX6 Quad core). I am try to SDIO driver and using&amp;nbsp;SD3 (J18 slot) as SD device, at datasheet level (not using linux or u-boot). For this purpose I configured SD3_CD (SD3_DAT5_PAD) to GPIO7_IO00. And I configured GPIO7 interrupt to edge trigger that whenever card inserted or removed, i should have the interrupt. But the problem is that when I insert or remove the card, I get almost 15-20 interrupts (may be due to debounce), So is there any hardware bit in or method to control the&amp;nbsp;debouncing affect on a pin. Thanks in advance. :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S: I can not modify my hardware, neither afford delay in the interrupt handler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Hamza&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Apr 2017 13:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-lite-SD3-Card-Detect-Pin-GPIO-debounce/m-p/641431#M97911</guid>
      <dc:creator>ameerhamza</dc:creator>
      <dc:date>2017-04-02T13:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre_lite SD3 Card Detect Pin (GPIO) debounce</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-lite-SD3-Card-Detect-Pin-GPIO-debounce/m-p/641432#M97912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hamza&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid i.MX6 GPIOs does not have hardware debounce support.&lt;/P&gt;&lt;P&gt;One can look at pin description on AN5078 Influence of Pin Setting on System Function and Performance&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf" title="http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Apr 2017 23:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-lite-SD3-Card-Detect-Pin-GPIO-debounce/m-p/641432#M97912</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-02T23:23:24Z</dc:date>
    </item>
  </channel>
</rss>