<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to get a custom minimal kernel configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-get-a-custom-minimal-kernel-configuration/m-p/641403#M97902</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to get a minimal kernel runing on an embedded hardware. The machine cpu is NXP i.MX7, it should support,&lt;BR /&gt;I2C&lt;BR /&gt;USB device for micro SD Card MSD mode&lt;BR /&gt;micro SD card, FAT file system&lt;BR /&gt;4.7 LCD with LCDIF&lt;BR /&gt;power management&lt;BR /&gt;video camera with MIPI DSI&lt;BR /&gt;matrix keypad&lt;BR /&gt;GPIO&lt;BR /&gt;ADC&lt;BR /&gt;PWM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system is set up to run qt program after power up. So I want to get a clean and minimal kernel configuration, only includes above sutffs, no network, no wifi, no bluetooth, etc, just keep the kernel as small as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone having the same experience how to make it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2017 05:34:21 GMT</pubDate>
    <dc:creator>leocheng</dc:creator>
    <dc:date>2017-01-24T05:34:21Z</dc:date>
    <item>
      <title>How to get a custom minimal kernel configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-get-a-custom-minimal-kernel-configuration/m-p/641403#M97902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to get a minimal kernel runing on an embedded hardware. The machine cpu is NXP i.MX7, it should support,&lt;BR /&gt;I2C&lt;BR /&gt;USB device for micro SD Card MSD mode&lt;BR /&gt;micro SD card, FAT file system&lt;BR /&gt;4.7 LCD with LCDIF&lt;BR /&gt;power management&lt;BR /&gt;video camera with MIPI DSI&lt;BR /&gt;matrix keypad&lt;BR /&gt;GPIO&lt;BR /&gt;ADC&lt;BR /&gt;PWM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system is set up to run qt program after power up. So I want to get a clean and minimal kernel configuration, only includes above sutffs, no network, no wifi, no bluetooth, etc, just keep the kernel as small as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone having the same experience how to make it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 05:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-get-a-custom-minimal-kernel-configuration/m-p/641403#M97902</guid>
      <dc:creator>leocheng</dc:creator>
      <dc:date>2017-01-24T05:34:21Z</dc:date>
    </item>
    <item>
      <title>Re: How to get a custom minimal kernel configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-get-a-custom-minimal-kernel-configuration/m-p/641404#M97903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can start with core-image-minimal configuration described&lt;/P&gt;&lt;P&gt;in Table 1. Freescale Yocto project images attached Yocto Guide.&lt;/P&gt;&lt;P&gt;Then include or exclude necessary modules using its description&lt;/P&gt;&lt;P&gt;in Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 07:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-get-a-custom-minimal-kernel-configuration/m-p/641404#M97903</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-24T07:14:02Z</dc:date>
    </item>
  </channel>
</rss>