<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 Hang during boot without UART cable connected in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641299#M97877</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably you need to place a pull-up resistor on the RX line, if that line has a low level the uart receiver may consider it as a character that needs to be received and this will overflow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a cable is connected to another device the the RX will have a high level when no data is available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Feb 2017 17:06:35 GMT</pubDate>
    <dc:creator>erdani80</dc:creator>
    <dc:date>2017-02-16T17:06:35Z</dc:date>
    <item>
      <title>iMX6 Hang during boot without UART cable connected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641297#M97875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a known issue with an iMX6 boot process hanging due to the UART? I have an intermittent problem on some boards where they only boot part-way until a UART cable is physically plugged in.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;They will spit out some Rx FIFO overrun errors for a while and then hang, e.g. here the bootup hung until a UART cable was connected 12 minutes later, at which point udevd etc started up:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[ 2.825049] imx-uart 21e8000.serial: Rx FIFO overrun&lt;BR /&gt;[ 3.584013] imx-uart 21e8000.serial: Rx FIFO overrun&lt;BR /&gt;[ 3.599746] imx-uart 21e8000.serial: Rx FIFO overrun&lt;BR /&gt;[ 3.612704] imx-uart 21e8000.serial: Rx FIFO overrun&lt;BR /&gt;[ 3.629967] imx-uart 21e8000.serial: Rx FIFO overrun&lt;BR /&gt;[ 3.652768] imx-uart 21e8000.serial: Rx FIFO overrun&lt;BR /&gt;[ 746.789572] udevd[156]: starting version 182&lt;BR /&gt;[ 746.795362] imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've attached a full boot dmesg, where one can see the 12 minute pause before a UART cable was physically connected. After that udevd starts, networking starts etc.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336265"&gt;uarts.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 09:49:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641297#M97875</guid>
      <dc:creator>kal</dc:creator>
      <dc:date>2017-02-16T09:49:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Hang during boot without UART cable connected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641298#M97876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if uart rx line is floating or noisy, as this may cause&lt;/P&gt;&lt;P&gt;its overrun errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 10:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641298#M97876</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-16T10:20:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Hang during boot without UART cable connected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641299#M97877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably you need to place a pull-up resistor on the RX line, if that line has a low level the uart receiver may consider it as a character that needs to be received and this will overflow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a cable is connected to another device the the RX will have a high level when no data is available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 17:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Hang-during-boot-without-UART-cable-connected/m-p/641299#M97877</guid>
      <dc:creator>erdani80</dc:creator>
      <dc:date>2017-02-16T17:06:35Z</dc:date>
    </item>
  </channel>
</rss>