<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Regarding SDIO as I/O device in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-SDIO-as-I-O-device/m-p/641279#M97871</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using SMARC card based on iMX6 solo platform.&lt;/P&gt;&lt;P&gt;The pin outs from &amp;nbsp;the SMARC based card has &lt;STRONG&gt;CD and WP(as GPIO pins from iMX6)&lt;/STRONG&gt; along with CLK ,CMD and 4 Data lines.&lt;/P&gt;&lt;P&gt;So what will be the state of CD and WP if i am not using these line for my application.&lt;/P&gt;&lt;P&gt;If i am using SDIO as an I/O device is there any recommendation for data lines , cmd lines and clk .&lt;/P&gt;&lt;P&gt;because as per SDIO spec Data3 line need pull up.&lt;/P&gt;&lt;P&gt;I have attached the pins from SMARC card for your reference.&lt;/P&gt;&lt;P&gt;Kindly please confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ashutosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Feb 2017 07:46:54 GMT</pubDate>
    <dc:creator>ashutoshnahar</dc:creator>
    <dc:date>2017-02-16T07:46:54Z</dc:date>
    <item>
      <title>Regarding SDIO as I/O device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-SDIO-as-I-O-device/m-p/641279#M97871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using SMARC card based on iMX6 solo platform.&lt;/P&gt;&lt;P&gt;The pin outs from &amp;nbsp;the SMARC based card has &lt;STRONG&gt;CD and WP(as GPIO pins from iMX6)&lt;/STRONG&gt; along with CLK ,CMD and 4 Data lines.&lt;/P&gt;&lt;P&gt;So what will be the state of CD and WP if i am not using these line for my application.&lt;/P&gt;&lt;P&gt;If i am using SDIO as an I/O device is there any recommendation for data lines , cmd lines and clk .&lt;/P&gt;&lt;P&gt;because as per SDIO spec Data3 line need pull up.&lt;/P&gt;&lt;P&gt;I have attached the pins from SMARC card for your reference.&lt;/P&gt;&lt;P&gt;Kindly please confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ashutosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 07:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Regarding-SDIO-as-I-O-device/m-p/641279#M97871</guid>
      <dc:creator>ashutoshnahar</dc:creator>
      <dc:date>2017-02-16T07:46:54Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding SDIO as I/O device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Regarding-SDIO-as-I-O-device/m-p/641280#M97872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. So what will be the state of CD and WP if i am not using these line for my application.&lt;/P&gt;&lt;P&gt;A. Both these pins should be tied to GND on the i.MX6 side.&lt;/P&gt;&lt;P&gt;Q. If i am using SDIO as an I/O device is there any recommendation for data lines , cmd lines and clk .&lt;/P&gt;&lt;P&gt;A. No external pull-ups/pull-downs are required on the data/cmd/clk lines for normal SDIO operation.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 09:12:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Regarding-SDIO-as-I-O-device/m-p/641280#M97872</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-02-21T09:12:28Z</dc:date>
    </item>
  </channel>
</rss>