<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX6 UL: loading image on OCRAM using Mfg tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641229#M97845</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the quick reply. &amp;nbsp;Is it possible to load a piece of code on OCRAM using manufacturing tool to get the board from brick to configured state? Then I can use the configure state to load image on External RAM or other boot devices.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Dec 2016 16:40:02 GMT</pubDate>
    <dc:creator>prabhatkumar</dc:creator>
    <dc:date>2016-12-02T16:40:02Z</dc:date>
    <item>
      <title>i.MX6 UL: loading image on OCRAM using Mfg tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641227#M97843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using i.MX6 UL EVK dev kit. I was wondering, how to load u-boot image on OCRAM using Mfg tool. I can't find any document related to this. &amp;nbsp;I would like to test this on the dev kit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 20:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641227#M97843</guid>
      <dc:creator>prabhatkumar</dc:creator>
      <dc:date>2016-12-01T20:33:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 UL: loading image on OCRAM using Mfg tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641228#M97844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We do not have OCRAM image of U_boot, at least because&lt;/P&gt;&lt;P&gt;of size : U-boot takes about 400 KB, OCRAM size is 128 KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2016 07:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641228#M97844</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-12-02T07:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 UL: loading image on OCRAM using Mfg tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641229#M97845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the quick reply. &amp;nbsp;Is it possible to load a piece of code on OCRAM using manufacturing tool to get the board from brick to configured state? Then I can use the configure state to load image on External RAM or other boot devices.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2016 16:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641229#M97845</guid>
      <dc:creator>prabhatkumar</dc:creator>
      <dc:date>2016-12-02T16:40:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 UL: loading image on OCRAM using Mfg tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641230#M97846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, basically it is possible to load a piece of code on OCRAM using manufacturing&lt;BR /&gt;tool. At least two points should be taken here for careful considerations :&lt;BR /&gt;1) loaded image should contain the IVT ;&lt;BR /&gt;2) OCRAM in itself used by boot ROM during load, therefore&lt;BR /&gt;&amp;nbsp;&amp;nbsp; only area, mentioned as "OCRAM Free Area" in i.MX6 RM, section&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 8.4.1 (Internal ROM /RAM memory map) is available for application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309765"&gt;u-boot.bin and u-boot.imx&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, please look at "Manufacturing Tool V2 UCL User Guide.docx" in MFG documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 06:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UL-loading-image-on-OCRAM-using-Mfg-tool/m-p/641230#M97846</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-12-05T06:10:14Z</dc:date>
    </item>
  </channel>
</rss>