<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: U-boot sf read max speed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641220#M97842</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there a patch for u-boot-imx6 to support faster speed than it is now. &lt;/P&gt;&lt;P&gt;We have custom board based on imx6 dual processor. I have read in the &lt;/P&gt;&lt;P&gt;forum that imx6 family processor does not support quad speed. So is &lt;/P&gt;&lt;P&gt;there possibility to support some other speed configuration that is &lt;/P&gt;&lt;P&gt;faster than this. I did not try official software because my board has &lt;/P&gt;&lt;P&gt;specific configuration od dts files and also u-boot configuration so &lt;/P&gt;&lt;P&gt;official software probably would not work. By the way what is maximum &lt;/P&gt;&lt;P&gt;speed of u-boot loader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, regards, Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Sep 2016 11:26:13 GMT</pubDate>
    <dc:creator>ivanljubicic</dc:creator>
    <dc:date>2016-09-23T11:26:13Z</dc:date>
    <item>
      <title>U-boot sf read max speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641218#M97840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have board which loads filesystem and kernel to RAM from spi flash when booting, because we do not want to use sd card for filesystem and kernel. It is 45 Mbytes big and it needs about 25 sec to be read with &lt;STRONG&gt;sf read &lt;/STRONG&gt;command to RAM. I have tried to speed up but I could not find the right solution. Spi flash is The Cypress S25FL512S and it is big 64 MBytes and in documentation it has max speed Quad Read Speed (SDR) of 52 MB/s. How can I setup in boot that I have such speed. I tried to increase the clock:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;CONFIG_SF_DEFAULT_SPEED&lt;/STRONG&gt; = 100000000&lt;/P&gt;&lt;P&gt;but it fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am stuck with it. The boot time is about 30s, and it should be 5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, regards, Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 16:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641218#M97840</guid>
      <dc:creator>ivanljubicic</dc:creator>
      <dc:date>2016-09-22T16:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot sf read max speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641219#M97841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Ivan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try to set &lt;STRONG&gt;CONFIG_SF_DEFAULT_SPEED&lt;/STRONG&gt; to&lt;/P&gt;&lt;P&gt;sensible value corresponding to datasheet spi chapter.&lt;/P&gt;&lt;P&gt;What processor used in the case, full marking. Not all&lt;/P&gt;&lt;P&gt;parts support quad spi mode. Try with official software from&lt;/P&gt;&lt;P&gt;i.MX6 product page&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW"&gt;i.MX 6 Series Software and Development Tool|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 00:03:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641219#M97841</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-23T00:03:15Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot sf read max speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641220#M97842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there a patch for u-boot-imx6 to support faster speed than it is now. &lt;/P&gt;&lt;P&gt;We have custom board based on imx6 dual processor. I have read in the &lt;/P&gt;&lt;P&gt;forum that imx6 family processor does not support quad speed. So is &lt;/P&gt;&lt;P&gt;there possibility to support some other speed configuration that is &lt;/P&gt;&lt;P&gt;faster than this. I did not try official software because my board has &lt;/P&gt;&lt;P&gt;specific configuration od dts files and also u-boot configuration so &lt;/P&gt;&lt;P&gt;official software probably would not work. By the way what is maximum &lt;/P&gt;&lt;P&gt;speed of u-boot loader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, regards, Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 11:26:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-sf-read-max-speed/m-p/641220#M97842</guid>
      <dc:creator>ivanljubicic</dc:creator>
      <dc:date>2016-09-23T11:26:13Z</dc:date>
    </item>
  </channel>
</rss>