<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow can I specify what kernel version to use when baking core-image-base?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-specify-what-kernel-version-to-use-when-baking-core/m-p/640678#M97715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to use a 4.1 kernel but whenever I bitbake core-image-base it results in a 3.14 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga&lt;SPAN style="color: #2b2b30; background-color: #dcf2fa;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;repo sync&lt;BR /&gt;MACHINE=imx6slevk source setup-environment imx6slevk/&lt;BR /&gt;bitbake core-image-base&lt;BR /&gt;&lt;BR /&gt;The resulting image has a 3.14.54-fslc+g94e5a3 kernel version. Anyone know why this happens or how to change the kernel version to 4.1.15-1.0.0?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Sep 2016 20:16:16 GMT</pubDate>
    <dc:creator>markcalhoun</dc:creator>
    <dc:date>2016-09-21T20:16:16Z</dc:date>
    <item>
      <title>How can I specify what kernel version to use when baking core-image-base?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-specify-what-kernel-version-to-use-when-baking-core/m-p/640678#M97715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to use a 4.1 kernel but whenever I bitbake core-image-base it results in a 3.14 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga&lt;SPAN style="color: #2b2b30; background-color: #dcf2fa;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;repo sync&lt;BR /&gt;MACHINE=imx6slevk source setup-environment imx6slevk/&lt;BR /&gt;bitbake core-image-base&lt;BR /&gt;&lt;BR /&gt;The resulting image has a 3.14.54-fslc+g94e5a3 kernel version. Anyone know why this happens or how to change the kernel version to 4.1.15-1.0.0?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 20:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-specify-what-kernel-version-to-use-when-baking-core/m-p/640678#M97715</guid>
      <dc:creator>markcalhoun</dc:creator>
      <dc:date>2016-09-21T20:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: How can I specify what kernel version to use when baking core-image-base?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-specify-what-kernel-version-to-use-when-baking-core/m-p/640679#M97716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; Please check if&amp;nbsp; NXP BSP Release options are used (not community&amp;nbsp; BSP), &lt;BR /&gt;which&amp;nbsp; are located in "meta-fsl-bsp-release" directory.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; Please follow recommendations of&amp;nbsp; "Freescale_Yocto_Project_User's_Guide.pdf".&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;&lt;BR /&gt;http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct &lt;BR /&gt;Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 01:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-specify-what-kernel-version-to-use-when-baking-core/m-p/640679#M97716</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-22T01:54:52Z</dc:date>
    </item>
  </channel>
</rss>