<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: linux/fb.h in the deploy-image differs from the one in kernel source tree in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/linux-fb-h-in-the-deploy-image-differs-from-the-one-in-kernel/m-p/639362#M97485</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;differencies may be explained by community BSP and official release BSPs as explained on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/402940#402940"&gt;https://community.freescale.com/message/402940#402940&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Mar 2017 23:00:56 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-03-12T23:00:56Z</dc:date>
    <item>
      <title>linux/fb.h in the deploy-image differs from the one in kernel source tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-fb-h-in-the-deploy-image-differs-from-the-one-in-kernel/m-p/639361#M97484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i just got involved in a project on a&amp;nbsp; board modified from imx6dlsabresd recently.&lt;/P&gt;&lt;P&gt;i have built the core-image-minimal and meta-toolchain&amp;nbsp; by yocto / bitbake with source from fsl-community-bsp 2.1.2 (kernel 4.1).&amp;nbsp;&lt;/P&gt;&lt;P&gt;when further worked on an application based on imx-test,&lt;/P&gt;&lt;P&gt;i found that the fb.h in build/tmp/sysroots/imx6dlsabresd/usr/include/linux differs from the one in kernel source.&lt;/P&gt;&lt;P&gt;can someone explain to me what the two versions are?&lt;/P&gt;&lt;P&gt;(i traced and found that when compiling imx-test with bitbake the real header file included is the "original" one from the kernel source : build/tmp/work-shared/imx6dlsabresd/kernel-source/include)&lt;/P&gt;&lt;P&gt;In addition, if we want to develop applications with but outside yocto, which "include"s and "lib"s in the build/tmp are the ones we should include / linked against?&lt;/P&gt;&lt;P&gt;paul wang.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Mar 2017 02:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-fb-h-in-the-deploy-image-differs-from-the-one-in-kernel/m-p/639361#M97484</guid>
      <dc:creator>balwang</dc:creator>
      <dc:date>2017-03-10T02:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: linux/fb.h in the deploy-image differs from the one in kernel source tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-fb-h-in-the-deploy-image-differs-from-the-one-in-kernel/m-p/639362#M97485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;differencies may be explained by community BSP and official release BSPs as explained on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/402940#402940"&gt;https://community.freescale.com/message/402940#402940&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Mar 2017 23:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-fb-h-in-the-deploy-image-differs-from-the-one-in-kernel/m-p/639362#M97485</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-12T23:00:56Z</dc:date>
    </item>
  </channel>
</rss>