<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIPI Virtual channel 1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Virtual-channel-1/m-p/638947#M97417</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;linux 3.0.35, imx6 dual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a mipi camera working on virtual channel 0 but I can't get it to work on any of the other virtual channels. Below is the board file setup I try to use for virtual channel 1. I may not have the mipi camera setup correctly but is there anything else I would need to change on the imx6 side? The mipi camera chip is Toshiba TC358746&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I run the mxc_v4l2_still.out utilitly I get:&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: mxc_v4l_read timeout counter 0&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: Not a CSI channel&lt;BR /&gt;v4l2 read error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static struct mipi_csi2_platform_data mipi_csi2_pdata = {&lt;BR /&gt; .ipu_id = 0,&lt;BR /&gt; .csi_id = 1,&lt;BR /&gt; .v_channel = 1,&lt;BR /&gt; .lanes = 2,&lt;BR /&gt; .dphy_clk = "mipi_pllref_clk",&lt;BR /&gt; .pixel_clk = "emi_clk",&lt;BR /&gt; .init = ghi_csi2_io_init,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static struct fsl_mxc_capture_platform_data capture_data[] = {&lt;BR /&gt; .csi = 1,&lt;BR /&gt; .ipu = 0,&lt;BR /&gt; .mclk_source = 0,&lt;BR /&gt; .is_mipi = 1,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Apr 2017 21:58:29 GMT</pubDate>
    <dc:creator>joemenard</dc:creator>
    <dc:date>2017-04-24T21:58:29Z</dc:date>
    <item>
      <title>MIPI Virtual channel 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Virtual-channel-1/m-p/638947#M97417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;linux 3.0.35, imx6 dual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a mipi camera working on virtual channel 0 but I can't get it to work on any of the other virtual channels. Below is the board file setup I try to use for virtual channel 1. I may not have the mipi camera setup correctly but is there anything else I would need to change on the imx6 side? The mipi camera chip is Toshiba TC358746&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I run the mxc_v4l2_still.out utilitly I get:&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: mxc_v4l_read timeout counter 0&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: Not a CSI channel&lt;BR /&gt;v4l2 read error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static struct mipi_csi2_platform_data mipi_csi2_pdata = {&lt;BR /&gt; .ipu_id = 0,&lt;BR /&gt; .csi_id = 1,&lt;BR /&gt; .v_channel = 1,&lt;BR /&gt; .lanes = 2,&lt;BR /&gt; .dphy_clk = "mipi_pllref_clk",&lt;BR /&gt; .pixel_clk = "emi_clk",&lt;BR /&gt; .init = ghi_csi2_io_init,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static struct fsl_mxc_capture_platform_data capture_data[] = {&lt;BR /&gt; .csi = 1,&lt;BR /&gt; .ipu = 0,&lt;BR /&gt; .mclk_source = 0,&lt;BR /&gt; .is_mipi = 1,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 21:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-Virtual-channel-1/m-p/638947#M97417</guid>
      <dc:creator>joemenard</dc:creator>
      <dc:date>2017-04-24T21:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI Virtual channel 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Virtual-channel-1/m-p/638948#M97418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi joe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for L3.0.35 one can look at VC3 configuration example:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-102233"&gt;Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 06:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-Virtual-channel-1/m-p/638948#M97418</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-25T06:08:44Z</dc:date>
    </item>
  </channel>
</rss>