<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX6 Solo serial Boot - device compatibility in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638436#M97350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for the answer!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read this chapter carefully, and i also checked the reference design.&lt;/P&gt;&lt;P&gt;But the information given in the reference manual is very slim.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking for Information like this:&lt;/P&gt;&lt;P&gt;- Which clock polarity settings is the bootloader using?&lt;/P&gt;&lt;P&gt;- Which commands are used by the bootloader (which instruction must be supported by my ROM?)&lt;/P&gt;&lt;P&gt;- Does the bootloader check the Chip-ID? Are there restrictions?&lt;/P&gt;&lt;P&gt;- Does the bootloader use a reset instruction, or do i have to use a Chip with reset input?&lt;/P&gt;&lt;P&gt;Since I found several Threads with Serial NOR boot problems, I want to be 100% sure, the chosen ROM is compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there is no such information available, i will have to check the whole SPI manually.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 06:55:13 GMT</pubDate>
    <dc:creator>max123</dc:creator>
    <dc:date>2016-09-22T06:55:13Z</dc:date>
    <item>
      <title>I.MX6 Solo serial Boot - device compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638434#M97348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am currently designing a custom Board with i.MX6 Solo. The Board will boot via serial boot (internal boot mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now trying to find a suitable serial flash device for this task. I thought about using a Micron &lt;SPAN style="font-size: 10.0pt;"&gt;N25Q064A&lt;/SPAN&gt;. But I cannot find detailed information about the SPI-protocol used by the i.MX6 Bootloader or a list of supported serial flash devices.&lt;/P&gt;&lt;P&gt;Where can i find this information?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 13:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638434#M97348</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2016-09-21T13:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 Solo serial Boot - device compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638435#M97349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check sect.8.5.4 Serial ROM through SPI i.MX6SDL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Spi boot is supported on Sabre AI board and one can look at its schematic&lt;/P&gt;&lt;P&gt;Schematics (5)&lt;BR /&gt;Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards &lt;BR /&gt;Design files for Base Board (REV E)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Fsabre-development-system%2Fsabre-for-automotive-infotainment-based-on-the-i.mx-6-series%3ARDIMX6SABREAUTO%3Ffpsp%3D1%26tab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-for-automotive-infotainment-based-on-the-i.mx-6-series:RDIMX6SABREAUTO?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 23:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638435#M97349</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-21T23:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 Solo serial Boot - device compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638436#M97350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for the answer!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read this chapter carefully, and i also checked the reference design.&lt;/P&gt;&lt;P&gt;But the information given in the reference manual is very slim.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking for Information like this:&lt;/P&gt;&lt;P&gt;- Which clock polarity settings is the bootloader using?&lt;/P&gt;&lt;P&gt;- Which commands are used by the bootloader (which instruction must be supported by my ROM?)&lt;/P&gt;&lt;P&gt;- Does the bootloader check the Chip-ID? Are there restrictions?&lt;/P&gt;&lt;P&gt;- Does the bootloader use a reset instruction, or do i have to use a Chip with reset input?&lt;/P&gt;&lt;P&gt;Since I found several Threads with Serial NOR boot problems, I want to be 100% sure, the chosen ROM is compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there is no such information available, i will have to check the whole SPI manually.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 06:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638436#M97350</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2016-09-22T06:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 Solo serial Boot - device compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638437#M97351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not aware of more detailed description than provided in RM.&lt;/P&gt;&lt;P&gt;In general one can configure processor for Serial NOR boot then stop&lt;/P&gt;&lt;P&gt;and check settings with jtag, ROM does not check Chip-ID.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 08:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Solo-serial-Boot-device-compatibility/m-p/638437#M97351</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-22T08:43:18Z</dc:date>
    </item>
  </channel>
</rss>