<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MuRata 1DX as Acess Point  in i.MX6 is invisible in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638385#M97332</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;SPAN style="color: #1c1c1c; background-color: #cce8cc;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="292717" data-username="jerseyyang" href="https://community.nxp.com/people/jerseyyang" style="color: #5e89c1; background-color: #cce8cc; border: 0px; font-weight: 600; text-decoration: none; font-size: 11.9994px;"&gt;jersey yang&lt;/A&gt;&lt;SPAN style="color: #1c1c1c; background-color: #cce8cc;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I face the same issue on Renesas R-car with Murata module. My issue is same with you. The AP is setup, but the AP ssid can not be scanned. I found the solution: insmod the bcmdhd.ko with option "op_mode=2".&lt;/P&gt;&lt;P&gt;The root cause is that the "op_mode" is initialized as 0, when setup AP mode "wl_cfg80211_start_ap()", it will check, then failed. However, set 2 to op_mode by your command "&lt;SPAN style="color: #1c1c1c; background-color: #cce8cc;"&gt;echo 2 &amp;gt; /sys/module/bcmdhd/parameters/op_mode&lt;/SPAN&gt;" does not work. I found use "op_mode=2" when insmod driver works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My analysis is as following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) "&lt;SPAN&gt;CFG80211-ERROR) check_dev_role_integrity : device role select failed" shows failed,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;static bool check_dev_role_integrity(struct bcm_cfg80211 *cfg, u32 dev_role)&lt;BR /&gt;{&lt;BR /&gt; dhd_pub_t *dhd = (dhd_pub_t *)(cfg-&amp;gt;pub);&lt;BR /&gt; if (((dev_role == NL80211_IFTYPE_AP) &amp;amp;&amp;amp;&lt;BR /&gt; !(dhd-&amp;gt;op_mode &amp;amp; DHD_FLAG_HOSTAP_MODE)) ||&lt;BR /&gt; ((dev_role == NL80211_IFTYPE_P2P_GO) &amp;amp;&amp;amp;&lt;BR /&gt; !(dhd-&amp;gt;op_mode &amp;amp; DHD_FLAG_P2P_GO_MODE)))&lt;BR /&gt; {&lt;BR /&gt; WL_ERR(("device role select failed\n"));&lt;BR /&gt; return false;&lt;BR /&gt; }&lt;BR /&gt; return true;&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error is the "op_mode" error, initialized value 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) "op_mode" is a module parameter, so just set a value when insmod the driver.&lt;/P&gt;&lt;P&gt;module_param(op_mode, int, 0644);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following is my log:&lt;/P&gt;&lt;P&gt;1) error log using "insmod /lib/modules/bcmdhd.ko firmware_path=/etc/firmware/fw_bcmdhd.bin nvram_path=/etc/firmware/bcmdhd.cal &lt;SPAN&gt;dhd_msg_level=0&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hostapd /etc/hostapd/hostapd_wps_wpa_11g.conf -B&lt;BR /&gt;Configuration file: /etc/hostapd/hostapd_wps_wpa_11g.conf&lt;BR /&gt;rfkill: Cannot open RFKILL control device&lt;BR /&gt;nl80211: Could not re-add multicast membership for vendor events: -2 (No such file orCFG80211-ERROR) wl_cfg80211_del_station : directory)&lt;BR /&gt;wlaDisconnect STA : ff:ff:ff:ff:ff:ff scb_val.val 3&lt;BR /&gt;n0: interface state UNINITIALIZED-&amp;gt;COUNTRY_UPDATE&lt;BR /&gt;Using interface wlan0 with hwaddr 00:90:4c:55:66:77 and ssid "murata_test"&lt;BR /&gt;CFG80211-ERROR) check_dev_role_integrity : device role select failed&lt;BR /&gt;wlan0: interface state COUNTRY_UPDATE-&amp;gt;ENABLED&lt;BR /&gt;wlan0: AP-ENABLED&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Correct log using "insmod /lib/modules/bcmdhd.ko firmware_path=/etc/firmware/fw_bcmdhd.bin nvram_path=/etc/firmware/bcmdhd.cal dhd_msg_level=0 op_mode=2"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@ale6:~# hostapd /etc/hostapd/hostapd_wps_wpa_11g.conf -B&lt;BR /&gt;Configuration file: /etc/hostapd/hostapd_wps_wpa_11g.conf&lt;BR /&gt;rfkill: Cannot open RFKILL control device&lt;BR /&gt;nl80211: Could not re-add multicast membership for vecfg80211: Calling CRDA for country: US&lt;BR /&gt;ndor events: -2 CFG80211-ERROR) wl_cfg80211_reg_notifier : (No such file or directoSet country code US from User&lt;BR /&gt;ry)&lt;BR /&gt;wlan0: interface state UNINITIALIZED-&amp;gt;COUNTRY_UPDATE&lt;BR /&gt;cfg80211: Regulatory domain changed to country: US&lt;BR /&gt;cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)&lt;BR /&gt;cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (3000 mBi, 0 mBm)&lt;BR /&gt;cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz), (1700 mBi, 0 mBm)&lt;BR /&gt;cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (3000 mBi, 0 mBm)&lt;BR /&gt;cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (4000 mBi, 0 mBm)&lt;BR /&gt;CFG80211-ERROR) wl_cfg80211_del_station : Disconnect STA : ff:ff:ff:ff:ff:ff scb_val.val 3&lt;BR /&gt;root@ale6:~# CFG80211-ERROR) wl_cfg80211_set_channel : netdev_ifidx(5), chan_type(1) target channel(2)&lt;BR /&gt;CFG80211-ERROR) wl_cfg80211_parse_ies : No WPSIE in beacon&lt;BR /&gt;CFG80211-ERROR) wl_cfg80211_parse_ies : No WPSIE in beacon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then my AP &lt;SPAN&gt;ssid "murata_test" is found by phone wifi scan.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 25 Nov 2017 03:54:38 GMT</pubDate>
    <dc:creator>westbrook</dc:creator>
    <dc:date>2017-11-25T03:54:38Z</dc:date>
    <item>
      <title>MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638379#M97326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone, &amp;nbsp;i am using the MuRata 1DX as WiFi module implementing the WIFI Hot-Spot in IMX6ULEVK board, now i come across some issues when i start up the hostapd serivce. it seems the AP mode is enabled, but i use another device as client and try to acess into the hot-spot(SSID:MuRata), but i cannot detect it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;here is the debug information:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;random: Trying to read entropy from /dev/random&lt;BR /&gt;Configuration file: /etc/hostapd.conf&lt;BR /&gt;ctrl_interface_group=0&lt;BR /&gt;rfkill: initial event: idx=0 type=1 op=0 soft=0 hard=0&lt;BR /&gt;rfkill: initial event: idx=1 type=1 op=0 soft=0 hard=0&lt;BR /&gt;nl80211: Using driver-based roaming&lt;BR /&gt;nl80211: TD_dhd_wlfc_mac_entry_update():1649, entry(32)&lt;BR /&gt;LS supported&lt;BR /&gt;nl80211: Supported cipher 00-0f-ac:1&lt;BR /&gt;nl80211: Supported cipher 00-0f-ac:5&lt;BR /&gt;nl80211: Supported cipher 00-0f-ac:2&lt;BR /&gt;nl80211: Supported cipher 00-0f-ac:4&lt;BR /&gt;nl80211: Supported cipher 00-0f-ac:6&lt;BR /&gt;nl80211: Using driver-based off-channel TX&lt;BR /&gt;nl80211: Supported vendor command: vendor_id=0x1018 subcmd=1&lt;BR /&gt;nl80211: Supported vendor event: vendor_id=0x1018 subcmd=0&lt;BR /&gt;nl80211: SupporCFG80211-ERROR) wl_cfg80211_del_station : ted vendor event: vendor_id=0x101Disconnect STA : ff:ff:ff:ff:ff:ff scb_val.val 3&lt;BR /&gt;8 subcmd=1&lt;BR /&gt;nl80211: Use separate P2P group interface (driver advertised support)&lt;BR /&gt;nl80211: Enable multi-channel concurrent (driver advertised support)&lt;BR /&gt;nl80211: Disable use_monitor with device_ap_sme since no monitor mode support detected&lt;BR /&gt;nl80211: interface wlan0 in phy phy0&lt;BR /&gt;nl80211: Set mode ifindex 7 iftype 3 (AP)&lt;BR /&gt;nl80211: Setup AP(wlan0) - device_ap_sme=1 use_monitor=0&lt;BR /&gt;nl80211: Subscribe to mgmt frames with AP handle 0x8b4918 (device SME)&lt;BR /&gt;nl80211: Register frame type=0xd0 nl_handle=0x8b4918 match=&lt;BR /&gt;nl80211: Enable Probe Request reporting nl_preq=0x8b48d0&lt;BR /&gt;nl80211: Register frame type=0x40 nl_handle=0x8b48d0 match=&lt;BR /&gt;nl80211: Add own interface ifindex 7&lt;BR /&gt;nl80211: if_indices[16]: 7&lt;BR /&gt;nl80211: Do not indicate P2P_DEVICE support (p2p_device=1 driver param not specified)&lt;BR /&gt;phy: phy0&lt;BR /&gt;BSS count 1, BSSID mask 00:00:00:00:00:00 (0 bits)&lt;BR /&gt;nl80211: Regulatory information - country=00&lt;BR /&gt;nl80211: 2402-2472 @ 40 MHz 20 mBm&lt;BR /&gt;nl80211: 2457-2482 @ 40 MHz 20 mBm (no IR)&lt;BR /&gt;nl80211: 2474-2494 @ 20 MHz 20 mBm (no OFDM) (no IR)&lt;BR /&gt;nl80211: 5170-5250 @ 160 MHz 20 mBm (no IR)&lt;BR /&gt;nl80211: 5250-5330 @ 160 MHz 20 mBm (DFS) (no IR)&lt;BR /&gt;nl80211: 5490-5730 @ 160 MHz 20 mBm (DFS) (no IR)&lt;BR /&gt;nl80211: Added 802.11b mode based on 802.11g information&lt;BR /&gt;Allowed channel: mode=1 chan=1 freq=2412 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=2 freq=2417 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=3 freq=2422 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=4 freq=2427 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=5 freq=2432 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=6 freq=2437 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=7 freq=2442 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=8 freq=2447 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=9 freq=2452 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=10 freq=2457 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=1 chan=11 freq=2462 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=1 freq=2412 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=2 freq=2417 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=3 freq=2422 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=4 freq=2427 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=5 freq=2432 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=6 freq=2437 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=7 freq=2442 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=8 freq=2447 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=9 freq=2452 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=10 freq=2457 MHz max_tx_power=20 dBm&lt;BR /&gt;Allowed channel: mode=0 chan=11 freq=2462 MHz max_tx_power=20 dBm&lt;BR /&gt;Completing interface initialization&lt;BR /&gt;Mode: IEEE 802.11g Channel: 2 Frequency: 2417 MHz&lt;BR /&gt;DFS 0 channels required radar detection&lt;BR /&gt;nl80211: Set freq 2417 (ht_enabled=1, vht_enabled=0, bandwidth=20 MHz, cf1=2417 MHz, cf2=0 MHz)&lt;BR /&gt;RATE[0] rate=10 flags=0x1&lt;BR /&gt;RATE[1] rate=20 flags=0x1&lt;BR /&gt;RATE[2] rate=55 flags=0x1&lt;BR /&gt;RATE[3] rate=110 flags=0x1&lt;BR /&gt;RATE[4] rate=60 flags=0x0&lt;BR /&gt;RATE[5] rate=90 flags=0x0&lt;BR /&gt;RATE[6] rate=120 flags=0x0&lt;BR /&gt;RATE[7] rate=180 flags=0x0&lt;BR /&gt;RATE[8] rate=240 flags=0x0&lt;BR /&gt;RATE[9] rate=360 flags=0x0&lt;BR /&gt;RATE[10] rate=480 flags=0x0&lt;BR /&gt;RATE[11] rate=540 flags=0x0&lt;BR /&gt;hostapd_setup_bss(hapd=0x8b3ec8 (wlan0), first=1)&lt;BR /&gt;wlan0: Flushing old station entries&lt;BR /&gt;nl80211: flush -&amp;gt; DEL_STATION wlan0 (all)&lt;BR /&gt;wlan0: Deauthenticate all stations&lt;BR /&gt;nl80211: sta_remove -&amp;gt; DEL_STATION wlan0 ff:ff:ff:ff:ff:ff --&amp;gt; 0 (Success)&lt;BR /&gt;wpa_driver_nl80211_set_key: ifindex=7 (wlan0) alg=0 addr=(nil) key_idx=0 set_tx=0 seq_len=0 key_len=0&lt;BR /&gt;wpa_driver_nl80211_set_key: ifindex=7 (wlan0) alg=0 addr=(nil) key_idx=1 set_tx=0 seq_len=0 key_len=0&lt;BR /&gt;wpa_driver_nl80211_set_key: ifindex=7 (wlan0) alg=0 addr=(nil) key_idx=2 set_tx=0 seq_len=0 key_len=0&lt;BR /&gt;wpa_driver_nl80211_set_key: ifindex=7 (wlan0) alg=0 addr=(nil) key_idx=3 set_tx=0 seq_len=0 key_len=0&lt;BR /&gt;Using interface wlan0 with hwaddCFG80211-ERROR) check_dev_role_integrity : r 60:f1:89:35:36:ca and ssid "MuRdevice role select failed&lt;BR /&gt;ata"&lt;BR /&gt;nl80211: Set beacon (beacon_set=0)&lt;BR /&gt;nl80211: Beacon head - hexdump(len=57): 80 00 00 00 ff ff ff ff ff ff 60 f1 89 35 36 ca 60 f1 89 35 36 ca 00 00 00 00 00 00 00 00 00 00 64 00 01 04 00 06 4d 75 52 61 74 61 01 08 82 84 8b 96 0c 12 18 24 03 01 02&lt;BR /&gt;nl80211: Beacon tail - hexdump(len=87): 2a 01 04 32 04 30 48 60 6c 2d 1a 0c 00 1f ff 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 3d 16 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 dd 18 00 50 f2 02 01 01 00 00 03 a4 00 00 27 a4 00 00 42 43 5e 00 62 32 2f 00&lt;BR /&gt;nl80211: ifindex=7&lt;BR /&gt;nl80211: beacon_int=100&lt;BR /&gt;nl80211: dtim_period=2&lt;BR /&gt;nl80211: ssid - hexdump_ascii(len=6):&lt;BR /&gt; 4d 75 52 61 74 61 MuRata &lt;BR /&gt;nl80211: hidden SSID not in use&lt;BR /&gt;nl80211: privacy=0&lt;BR /&gt;nl80211: auth_algs=0x1&lt;BR /&gt;nl80211: wpa_version=0x0&lt;BR /&gt;nl80211: key_mgmt_suites=0x2&lt;BR /&gt;nl80211: pairwise_ciphers=0x1&lt;BR /&gt;nl80211: group_cipher=0x1&lt;BR /&gt;nl80211: Set wlan0 operstate 0-&amp;gt;1 (UP)&lt;BR /&gt;netlink: Operstate: ifindex=7 linkmode=-1 (no change), operstate=6 (IF_OPER_UP)&lt;BR /&gt;Failed to set TX queue parameters for queue 0.&lt;BR /&gt;Failed to set TX queue parameters for queue 1.&lt;BR /&gt;Failed to set TX queue parameters for queue 2.&lt;BR /&gt;Failed to set TX queue parameters for queue 3.&lt;BR /&gt;wlan0: interface state UNINITIALIZED-&amp;gt;ENABLED&lt;BR /&gt;wlan0: AP-ENABLED &lt;BR /&gt;wlan0: Setup of interface done.&lt;BR /&gt;ctrl_iface not configured!&lt;BR /&gt;root@imx6ulevk:/tmp/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;before i start up the hostapd service, i insmod the bcmdhd.ko and configure the dhcpd.conf/dchp-server, iptables,&amp;nbsp;&lt;/P&gt;&lt;P&gt;the insmod command like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;insmod /home/root/bcmdhd.ko firmware_path=/lib/firmware/bcm/fw_bcmdhd.bin nvram_path=/lib/firmware/bcm/bcmdhd.1DX.SDIO.cal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i put the fw_bcmdhd.bin and&amp;nbsp;&lt;SPAN&gt;bcmdhd.1DX.SDIO.cal into the path /lib/firmware/bcm/ and locate the bcmdhd.ko in the /home/root/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;also, i exute this command to confiure the driver as AP mode:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;echo 2 &amp;gt; /sys/module/bcmdhd/parameters/op_mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;one more thing, before i debug the Acess-Point function, i start up the wpa_supplicant service, it works normally. i can use the imx6ulevk as client to ping another IP in the local network via wireless port(wlan0), the AP mode, use the same&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the interfaces configure like this:&lt;/SPAN&gt;&lt;BR /&gt;auto lo&lt;BR /&gt;iface lo inet loopback&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;iface wlan0 inet static&lt;BR /&gt;address 10.163.44.145&lt;BR /&gt;netmask 255.255.255.0&lt;BR /&gt;gateway 10.163.44.245&lt;/P&gt;&lt;P&gt;iface atml0 inet dhcp&lt;/P&gt;&lt;P&gt;# Wired or wireless interfaces&lt;BR /&gt;auto eth0&lt;BR /&gt;iface eth0 inet dhcp&lt;BR /&gt;iface eth1 inet dhcp&lt;/P&gt;&lt;P&gt;# Ethernet/RNDIS gadget (g_ether)&lt;BR /&gt;# ... or on host side, usbnet and random hwaddr&lt;BR /&gt;iface usb0 inet static&lt;BR /&gt; address 192.168.7.2&lt;BR /&gt; netmask 255.255.255.0&lt;BR /&gt; network 192.168.7.0&lt;BR /&gt; gateway 192.168.7.1&lt;/P&gt;&lt;P&gt;# Bluetooth networking&lt;BR /&gt;iface bnep0 inet dhcp&lt;BR /&gt;pre-up iptables-restore &amp;lt; /etc/iptables.ipv4.nat&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the hostapd.conf configure like this:&lt;/P&gt;&lt;P&gt;interface=wlan0&lt;BR /&gt;logger_syslog=-1&lt;BR /&gt;logger_syslog_level=4&lt;BR /&gt;logger_stdout=-1&lt;BR /&gt;logger_stdout_level=4&lt;BR /&gt;ctrl_interface=/var/run/hostapd&lt;BR /&gt;ctrl_interface_group=0&lt;BR /&gt;ssid=MuRata&lt;BR /&gt;hw_mode=g&lt;BR /&gt;channel=2&lt;BR /&gt;beacon_int=100&lt;BR /&gt;dtim_period=2&lt;BR /&gt;max_num_sta=255&lt;BR /&gt;rts_threshold=2347&lt;BR /&gt;fragm_threshold=2346&lt;BR /&gt;macaddr_acl=0&lt;BR /&gt;auth_algs=1&lt;BR /&gt;ignore_broadcast_ssid=0&lt;BR /&gt;wmm_enabled=1&lt;BR /&gt;wmm_ac_bk_cwmin=4&lt;BR /&gt;wmm_ac_bk_cwmax=10&lt;BR /&gt;wmm_ac_bk_aifs=7&lt;BR /&gt;wmm_ac_bk_txop_limit=0&lt;BR /&gt;wmm_ac_bk_acm=0&lt;BR /&gt;wmm_ac_be_aifs=3&lt;BR /&gt;wmm_ac_be_cwmin=4&lt;BR /&gt;wmm_ac_be_cwmax=10&lt;BR /&gt;wmm_ac_be_txop_limit=0&lt;BR /&gt;wmm_ac_be_acm=0&lt;BR /&gt;wmm_ac_vi_aifs=2&lt;BR /&gt;wmm_ac_vi_cwmin=3&lt;BR /&gt;wmm_ac_vi_cwmax=4&lt;BR /&gt;wmm_ac_vi_txop_limit=94&lt;BR /&gt;wmm_ac_vi_acm=0&lt;BR /&gt;wmm_ac_vo_aifs=2&lt;BR /&gt;wmm_ac_vo_cwmin=2&lt;BR /&gt;wmm_ac_vo_cwmax=3&lt;BR /&gt;wmm_ac_vo_txop_limit=47&lt;BR /&gt;wmm_ac_vo_acm=0&lt;BR /&gt;eapol_key_index_workaround=0&lt;BR /&gt;eap_server=0&lt;BR /&gt;own_ip_addr=127.0.0.1&lt;BR /&gt;driver=nl80211&lt;BR /&gt;ieee80211n=1&lt;BR /&gt;rsn_pairwise=CCMP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does anybody encounter the similar issue? and how do you fix it? Note: all of this runs in the linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 09:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638379#M97326</guid>
      <dc:creator>jerseyyang</dc:creator>
      <dc:date>2017-03-09T09:27:05Z</dc:date>
    </item>
    <item>
      <title>Re: MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638380#M97327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think this is a configuration issue of MuRata wifi module.&lt;/P&gt;&lt;P&gt;Please visit this link : &lt;A class="link-titled" href="http://wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-nxp-i-mx.html" title="http://wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-nxp-i-mx.html"&gt;Wi-Fi Bluetooth for NXP i.MX | RF Modules | Wireless Products | Murata Manufacturing | Murata Manufacturing&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 07:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638380#M97327</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-03-16T07:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638381#M97328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what do you mean? jimmy, i just follow the instruction of that guide.&amp;nbsp; i heard from other guys, the fw_bcmdhd.bin just support station mode, so i got another fw_bcmdhd_apsta.bin, it always report this error, and the SSID not broadcast, also you did not point out what is the configuration issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 07:58:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638381#M97328</guid>
      <dc:creator>jerseyyang</dc:creator>
      <dc:date>2017-03-16T07:58:48Z</dc:date>
    </item>
    <item>
      <title>Re: MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638382#M97329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to contact MuRata for the better support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 08:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638382#M97329</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-03-16T08:08:04Z</dc:date>
    </item>
    <item>
      <title>Re: MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638383#M97330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the fw_bcmdhd_apsta.bin supports the AP mode, just download the correct firmware to fix the issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 09:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638383#M97330</guid>
      <dc:creator>jerseyyang</dc:creator>
      <dc:date>2017-03-28T09:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638384#M97331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I'm having similar issues as well, might you be able to point me to the right place to download this bin file?&lt;BR /&gt;thanks :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 13:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638384#M97331</guid>
      <dc:creator>karunikajiayech</dc:creator>
      <dc:date>2017-10-13T13:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: MuRata 1DX as Acess Point  in i.MX6 is invisible</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638385#M97332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;SPAN style="color: #1c1c1c; background-color: #cce8cc;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="292717" data-username="jerseyyang" href="https://community.nxp.com/people/jerseyyang" style="color: #5e89c1; background-color: #cce8cc; border: 0px; font-weight: 600; text-decoration: none; font-size: 11.9994px;"&gt;jersey yang&lt;/A&gt;&lt;SPAN style="color: #1c1c1c; background-color: #cce8cc;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I face the same issue on Renesas R-car with Murata module. My issue is same with you. The AP is setup, but the AP ssid can not be scanned. I found the solution: insmod the bcmdhd.ko with option "op_mode=2".&lt;/P&gt;&lt;P&gt;The root cause is that the "op_mode" is initialized as 0, when setup AP mode "wl_cfg80211_start_ap()", it will check, then failed. However, set 2 to op_mode by your command "&lt;SPAN style="color: #1c1c1c; background-color: #cce8cc;"&gt;echo 2 &amp;gt; /sys/module/bcmdhd/parameters/op_mode&lt;/SPAN&gt;" does not work. I found use "op_mode=2" when insmod driver works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My analysis is as following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) "&lt;SPAN&gt;CFG80211-ERROR) check_dev_role_integrity : device role select failed" shows failed,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;static bool check_dev_role_integrity(struct bcm_cfg80211 *cfg, u32 dev_role)&lt;BR /&gt;{&lt;BR /&gt; dhd_pub_t *dhd = (dhd_pub_t *)(cfg-&amp;gt;pub);&lt;BR /&gt; if (((dev_role == NL80211_IFTYPE_AP) &amp;amp;&amp;amp;&lt;BR /&gt; !(dhd-&amp;gt;op_mode &amp;amp; DHD_FLAG_HOSTAP_MODE)) ||&lt;BR /&gt; ((dev_role == NL80211_IFTYPE_P2P_GO) &amp;amp;&amp;amp;&lt;BR /&gt; !(dhd-&amp;gt;op_mode &amp;amp; DHD_FLAG_P2P_GO_MODE)))&lt;BR /&gt; {&lt;BR /&gt; WL_ERR(("device role select failed\n"));&lt;BR /&gt; return false;&lt;BR /&gt; }&lt;BR /&gt; return true;&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error is the "op_mode" error, initialized value 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) "op_mode" is a module parameter, so just set a value when insmod the driver.&lt;/P&gt;&lt;P&gt;module_param(op_mode, int, 0644);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following is my log:&lt;/P&gt;&lt;P&gt;1) error log using "insmod /lib/modules/bcmdhd.ko firmware_path=/etc/firmware/fw_bcmdhd.bin nvram_path=/etc/firmware/bcmdhd.cal &lt;SPAN&gt;dhd_msg_level=0&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hostapd /etc/hostapd/hostapd_wps_wpa_11g.conf -B&lt;BR /&gt;Configuration file: /etc/hostapd/hostapd_wps_wpa_11g.conf&lt;BR /&gt;rfkill: Cannot open RFKILL control device&lt;BR /&gt;nl80211: Could not re-add multicast membership for vendor events: -2 (No such file orCFG80211-ERROR) wl_cfg80211_del_station : directory)&lt;BR /&gt;wlaDisconnect STA : ff:ff:ff:ff:ff:ff scb_val.val 3&lt;BR /&gt;n0: interface state UNINITIALIZED-&amp;gt;COUNTRY_UPDATE&lt;BR /&gt;Using interface wlan0 with hwaddr 00:90:4c:55:66:77 and ssid "murata_test"&lt;BR /&gt;CFG80211-ERROR) check_dev_role_integrity : device role select failed&lt;BR /&gt;wlan0: interface state COUNTRY_UPDATE-&amp;gt;ENABLED&lt;BR /&gt;wlan0: AP-ENABLED&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Correct log using "insmod /lib/modules/bcmdhd.ko firmware_path=/etc/firmware/fw_bcmdhd.bin nvram_path=/etc/firmware/bcmdhd.cal dhd_msg_level=0 op_mode=2"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@ale6:~# hostapd /etc/hostapd/hostapd_wps_wpa_11g.conf -B&lt;BR /&gt;Configuration file: /etc/hostapd/hostapd_wps_wpa_11g.conf&lt;BR /&gt;rfkill: Cannot open RFKILL control device&lt;BR /&gt;nl80211: Could not re-add multicast membership for vecfg80211: Calling CRDA for country: US&lt;BR /&gt;ndor events: -2 CFG80211-ERROR) wl_cfg80211_reg_notifier : (No such file or directoSet country code US from User&lt;BR /&gt;ry)&lt;BR /&gt;wlan0: interface state UNINITIALIZED-&amp;gt;COUNTRY_UPDATE&lt;BR /&gt;cfg80211: Regulatory domain changed to country: US&lt;BR /&gt;cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)&lt;BR /&gt;cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (3000 mBi, 0 mBm)&lt;BR /&gt;cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz), (1700 mBi, 0 mBm)&lt;BR /&gt;cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (3000 mBi, 0 mBm)&lt;BR /&gt;cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (4000 mBi, 0 mBm)&lt;BR /&gt;CFG80211-ERROR) wl_cfg80211_del_station : Disconnect STA : ff:ff:ff:ff:ff:ff scb_val.val 3&lt;BR /&gt;root@ale6:~# CFG80211-ERROR) wl_cfg80211_set_channel : netdev_ifidx(5), chan_type(1) target channel(2)&lt;BR /&gt;CFG80211-ERROR) wl_cfg80211_parse_ies : No WPSIE in beacon&lt;BR /&gt;CFG80211-ERROR) wl_cfg80211_parse_ies : No WPSIE in beacon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then my AP &lt;SPAN&gt;ssid "murata_test" is found by phone wifi scan.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Nov 2017 03:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MuRata-1DX-as-Acess-Point-in-i-MX6-is-invisible/m-p/638385#M97332</guid>
      <dc:creator>westbrook</dc:creator>
      <dc:date>2017-11-25T03:54:38Z</dc:date>
    </item>
  </channel>
</rss>