<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6DL - Determine Boot From Recovery Device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637997#M97238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we're building our own hardware based on an i.MX6DL using an eMMC as primary boot device and an SPI NOR Flash as&amp;nbsp;recovery&amp;nbsp;device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our board behaves as expected when there is no bootloader in eMMC,&amp;nbsp;i.e. it boots from&amp;nbsp;SPI NOR Flash, but I can find no&amp;nbsp;indication about that fact in&amp;nbsp;any of the SRC registers I've been looking at.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there such an&amp;nbsp;indication at all and - if so - where can I find it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chris.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Oct 2016 12:58:41 GMT</pubDate>
    <dc:creator>christian_neuwi</dc:creator>
    <dc:date>2016-10-14T12:58:41Z</dc:date>
    <item>
      <title>i.MX6DL - Determine Boot From Recovery Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637997#M97238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we're building our own hardware based on an i.MX6DL using an eMMC as primary boot device and an SPI NOR Flash as&amp;nbsp;recovery&amp;nbsp;device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our board behaves as expected when there is no bootloader in eMMC,&amp;nbsp;i.e. it boots from&amp;nbsp;SPI NOR Flash, but I can find no&amp;nbsp;indication about that fact in&amp;nbsp;any of the SRC registers I've been looking at.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there such an&amp;nbsp;indication at all and - if so - where can I find it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chris.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Oct 2016 12:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637997#M97238</guid>
      <dc:creator>christian_neuwi</dc:creator>
      <dc:date>2016-10-14T12:58:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL - Determine Boot From Recovery Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637998#M97239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid there is no such indication which recovery device was used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Oct 2016 23:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637998#M97239</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-14T23:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL - Determine Boot From Recovery Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637999#M97240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FYI:&lt;/P&gt;&lt;P&gt;The flag&amp;nbsp;PERSIST_SECONDARY_BOOT (SRC_GPR10[30]) does indicate that booting occurred from the&amp;nbsp;recovery device. It might not say exactly&amp;nbsp;&lt;STRONG&gt;which&lt;/STRONG&gt;&amp;nbsp;&lt;SPAN&gt;recovery device was used, but since you can have only one that information is usually good enough for the firmware to react appropriately if needed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Chris.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 16:17:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Determine-Boot-From-Recovery-Device/m-p/637999#M97240</guid>
      <dc:creator>christian_neuwi</dc:creator>
      <dc:date>2017-08-29T16:17:37Z</dc:date>
    </item>
  </channel>
</rss>