<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Multiplexing UART</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637404#M97120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Ours is a custom board is based on imx6.In which UART 2 is connected to GSM modem.In linux we are only able to access the UART once.What we wanted is to multiplex the UART 2 i.e ttymxc1 into 3 or 2 virtual port . So that i can access my serial port multiple times.Is there any driver available to multiplex my ttymxc1.If there is any method to multiplex please help me.Please reply as soon as possible&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Nov 2016 05:21:35 GMT</pubDate>
    <dc:creator>deepanrajanbara</dc:creator>
    <dc:date>2016-11-30T05:21:35Z</dc:date>
    <item>
      <title>Multiplexing UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637404#M97120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Ours is a custom board is based on imx6.In which UART 2 is connected to GSM modem.In linux we are only able to access the UART once.What we wanted is to multiplex the UART 2 i.e ttymxc1 into 3 or 2 virtual port . So that i can access my serial port multiple times.Is there any driver available to multiplex my ttymxc1.If there is any method to multiplex please help me.Please reply as soon as possible&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 05:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637404#M97120</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2016-11-30T05:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: Multiplexing UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637405#M97121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Linux we are having a GSM Mux line discipline support if we enable and follow the document in linux kernel i.e n_gsm.txt we are able to get virtual port of my ttymxc1.But now what problem is that when we try to "cat /dev/ttygsm1 " we are getting messgae "LEVEL 2 : Halted" what could be the issue can anyone help me in this issue .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 13:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637405#M97121</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2016-11-30T13:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: Multiplexing UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637406#M97122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean the access to a single hardware UART port by different processes/software threads at the same time? If so, the answer is: no, it is not possible. It is prohibited on the Linux kernel level.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2016 10:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiplexing-UART/m-p/637406#M97122</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-12-21T10:04:12Z</dc:date>
    </item>
  </channel>
</rss>