<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mfg tool - bootstrap and updater</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-bootstrap-and-updater/m-p/637187#M97064</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ran&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;files which uses mfg tools (it is its own image) are located in&lt;/P&gt;&lt;P&gt;..OS Firmware/firmware folder, files which will be programmed&lt;/P&gt;&lt;P&gt;to media (programmed to some storage device) - in ..OS Firmware/files&lt;/P&gt;&lt;P&gt;folder, also it is useful to check documents in /Document folder. Default&lt;/P&gt;&lt;P&gt;u-boot/kernel for mfg/tool is built for nxp reference boards, for custom board it&lt;/P&gt;&lt;P&gt;should be rebuilt, if custom board is identical to reference board, it may work&lt;/P&gt;&lt;P&gt;without rebuilding firmware files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Nov 2016 23:24:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-11-07T23:24:00Z</dc:date>
    <item>
      <title>mfg tool - bootstrap and updater</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-bootstrap-and-updater/m-p/637186#M97063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would please like to ask a question about mfg tool.&lt;/P&gt;&lt;P&gt;I've read the&amp;nbsp;documentation of mfg tool, and would please like to know:&lt;/P&gt;&lt;P&gt;1. According to documentation it requires that we dedicated u-boot &amp;amp; kernel for mfg tool, are these binaries should be programmed to the same storage device as the "updater" u-boot/kernel ?&lt;/P&gt;&lt;P&gt;2. When we update u-boot/kernel (updater), does it override the u-boot/kernel for mfg/tool ? If yes - why can't we use the u-boot/kernel for mfg tool, as &amp;nbsp;operational firmware u-boot/kernel ? (in such way we don't need the updater)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Nov 2016 14:21:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-bootstrap-and-updater/m-p/637186#M97063</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2016-11-07T14:21:05Z</dc:date>
    </item>
    <item>
      <title>Re: mfg tool - bootstrap and updater</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-bootstrap-and-updater/m-p/637187#M97064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ran&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;files which uses mfg tools (it is its own image) are located in&lt;/P&gt;&lt;P&gt;..OS Firmware/firmware folder, files which will be programmed&lt;/P&gt;&lt;P&gt;to media (programmed to some storage device) - in ..OS Firmware/files&lt;/P&gt;&lt;P&gt;folder, also it is useful to check documents in /Document folder. Default&lt;/P&gt;&lt;P&gt;u-boot/kernel for mfg/tool is built for nxp reference boards, for custom board it&lt;/P&gt;&lt;P&gt;should be rebuilt, if custom board is identical to reference board, it may work&lt;/P&gt;&lt;P&gt;without rebuilding firmware files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Nov 2016 23:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-bootstrap-and-updater/m-p/637187#M97064</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-07T23:24:00Z</dc:date>
    </item>
  </channel>
</rss>