<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issue booting Imx6 with 3.16 kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637132#M97053</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on imx6-sabresd board. I am trying to port linux kernel 3.16( from kernel.org) to board. I have used the link &lt;A href="https://community.nxp.com/docs/DOC-330147"&gt;https://community.nxp.com/docs/DOC-330147&lt;/A&gt; to set up u-boot, kernel and rootfs. I am able to boot board with u-boot.&lt;/P&gt;&lt;P&gt;But when it is starting kernel, it is trying to load rootfs from mmcblk0p2 instead of mmcblk2p2 which is my sdcard having rootfs.&amp;nbsp; I tried with kernel 3.14 from above page it is able to boot with no issues. Any guess why it is happening ? Is there something that needs to be done in kernel source code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Sep 2016 07:37:28 GMT</pubDate>
    <dc:creator>prathamrahate</dc:creator>
    <dc:date>2016-09-21T07:37:28Z</dc:date>
    <item>
      <title>Issue booting Imx6 with 3.16 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637132#M97053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on imx6-sabresd board. I am trying to port linux kernel 3.16( from kernel.org) to board. I have used the link &lt;A href="https://community.nxp.com/docs/DOC-330147"&gt;https://community.nxp.com/docs/DOC-330147&lt;/A&gt; to set up u-boot, kernel and rootfs. I am able to boot board with u-boot.&lt;/P&gt;&lt;P&gt;But when it is starting kernel, it is trying to load rootfs from mmcblk0p2 instead of mmcblk2p2 which is my sdcard having rootfs.&amp;nbsp; I tried with kernel 3.14 from above page it is able to boot with no issues. Any guess why it is happening ? Is there something that needs to be done in kernel source code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 07:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637132#M97053</guid>
      <dc:creator>prathamrahate</dc:creator>
      <dc:date>2016-09-21T07:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: Issue booting Imx6 with 3.16 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637133#M97054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you need to change&amp;nbsp;a U-boot enviroment variable value&amp;nbsp;from mmcblk0p2 to mmcblk2p2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 07:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637133#M97054</guid>
      <dc:creator>jan_spurek</dc:creator>
      <dc:date>2016-09-21T07:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: Issue booting Imx6 with 3.16 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637134#M97055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for reply. In u-boot, there is environment variable mmcdev, it default set to 1, If i change it to 2 then try to boot, it is working fine, no issues. But my question is why it is happening with 3.16 kernel only??&lt;/P&gt;&lt;P&gt;With 3.14 kernel i dont need to change mmcdev, it boots properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 08:05:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-booting-Imx6-with-3-16-kernel/m-p/637134#M97055</guid>
      <dc:creator>prathamrahate</dc:creator>
      <dc:date>2016-09-21T08:05:49Z</dc:date>
    </item>
  </channel>
</rss>