<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ODT setting for i.MX6UL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ODT-setting-for-i-MX6UL/m-p/636907#M97008</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Basically, ODT feature is intended for data DQ, data strobes DQS, and data masks DM.&lt;/P&gt;&lt;P&gt;Address and command lines are not affected by the ODT.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; The ODT field of DRAM_ADDRxx register relates only to address lines, and really should not be used. &lt;BR /&gt;The MMDC PHY ODT control register is applied to configure data DQ, data strobes DQS, and data masks &lt;BR /&gt;DM. This register is used really for ODT configuring.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, it is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Dec 2016 03:13:39 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-12-26T03:13:39Z</dc:date>
    <item>
      <title>ODT setting for i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ODT-setting-for-i-MX6UL/m-p/636906#M97007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am doing prelayout simulation for i.MX6UL processor with DDR3L.&lt;/P&gt;&lt;P&gt;However in Ref. manual I can see ODT available for all address and control lines.&lt;/P&gt;&lt;P&gt;Also in Hyperlynx for model selection I am not able to understand for processor why address line can be configured as input. The same is shown in attached figure.&lt;/P&gt;&lt;P&gt;I also could not find the list of ODT's available for data lines in reference manual. However I can see them in Hyperlynx model selector. The same shown in attached image.&lt;/P&gt;&lt;P&gt;Let me know if I am using the correct IBIS model for CPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Surendra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Dec 2016 06:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ODT-setting-for-i-MX6UL/m-p/636906#M97007</guid>
      <dc:creator>surendrajadhav</dc:creator>
      <dc:date>2016-12-23T06:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: ODT setting for i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ODT-setting-for-i-MX6UL/m-p/636907#M97008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Basically, ODT feature is intended for data DQ, data strobes DQS, and data masks DM.&lt;/P&gt;&lt;P&gt;Address and command lines are not affected by the ODT.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; The ODT field of DRAM_ADDRxx register relates only to address lines, and really should not be used. &lt;BR /&gt;The MMDC PHY ODT control register is applied to configure data DQ, data strobes DQS, and data masks &lt;BR /&gt;DM. This register is used really for ODT configuring.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, it is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Dec 2016 03:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ODT-setting-for-i-MX6UL/m-p/636907#M97008</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-12-26T03:13:39Z</dc:date>
    </item>
  </channel>
</rss>