<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636889#M96998</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So,turns out that I tried 3 other SD cards and same story.&amp;nbsp; I tried a SanDisk from my QP board and it boots!&lt;/P&gt;&lt;P&gt;What's up with SD cards and u-boot?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Sep 2016 19:13:30 GMT</pubDate>
    <dc:creator>jpe1313</dc:creator>
    <dc:date>2016-09-21T19:13:30Z</dc:date>
    <item>
      <title>i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636882#M96991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the&amp;nbsp;i.MX6 &amp;nbsp;SABRE MCIMX6Q-SDB&amp;nbsp;&amp;nbsp; out of the box the Android boots from the SC card but I need to use Yocto and I need a "core-image-base."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I utilized the MOST CURRENT (I think)&amp;nbsp;Freescale Yocto Project User's Guide, Rev. 0, 04/2016 and successfully got a "core-image-base-imx6qsabresd.sdcard"&amp;nbsp;&amp;nbsp; which is an&amp;nbsp;84.0 MB file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I image the SD card with dd as per section 6.1 Flashing an SD card image, I can see the following:&lt;/P&gt;&lt;P&gt;Boot imx6qs 8.4 MB FAT&amp;nbsp; - and that has&amp;nbsp; the "zImage" and the "imx6q-sabresd.dtb" file(s)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; on /dev/sdd1&lt;/P&gt;&lt;P&gt;and /dev/sdd2&amp;nbsp;&amp;nbsp; has the root file system.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the boot :&lt;/P&gt;&lt;P&gt;_____________________________________________________________________________&lt;/P&gt;&lt;P&gt;U-Boot 2015.04imx_v2015.04_4.1.15_1.2.0_ga+gede7538 (Sep 06 2016 - 17:19:19)&lt;/P&gt;&lt;P&gt;　&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.5 at 792 MHz&lt;/P&gt;&lt;P&gt;CPU: Temperature 24 C&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: MX6-SabreSD&lt;/P&gt;&lt;P&gt;I2C: ready&lt;/P&gt;&lt;P&gt;DRAM: 1 GiB&lt;/P&gt;&lt;P&gt;PMIC: PFUZE100 ID=0x10&lt;/P&gt;&lt;P&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/P&gt;&lt;P&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;　&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;/P&gt;&lt;P&gt;Display: Hannstar-XGA (1024x768)&lt;/P&gt;&lt;P&gt;In: serial&lt;/P&gt;&lt;P&gt;Out: serial&lt;/P&gt;&lt;P&gt;Err: serial&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;/P&gt;&lt;P&gt;mmc1 is current device&lt;/P&gt;&lt;P&gt;Net: FEC [PRIME]&lt;/P&gt;&lt;P&gt;Normal Boot&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;/P&gt;&lt;P&gt;mmc1 is current device&lt;/P&gt;&lt;P&gt;reading boot.scr&lt;/P&gt;&lt;P&gt;** Unable to read file boot.scr **&lt;/P&gt;&lt;P&gt;reading zImage&lt;/P&gt;&lt;P&gt;Error reading cluster&lt;/P&gt;&lt;P&gt;** Unable to read file zImage **&lt;/P&gt;&lt;P&gt;Booting from net ...&lt;/P&gt;&lt;P&gt;FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;/P&gt;&lt;P&gt;BOOTP broadcast 1&lt;/P&gt;&lt;P&gt;BOOTP broadcast 2&lt;/P&gt;&lt;P&gt;BOOTP broadcast 3&lt;/P&gt;&lt;P&gt;BOOTP broadcast 4&lt;/P&gt;&lt;P&gt;_____________________________________________________________________________&lt;/P&gt;&lt;P&gt;Oh, yes I checked and the SW6 on the board and it is set correctly - I.MX 6 SABRE-SD boards in the Linux User's Guide, Rev. L4.1.15_1.0.0-ga, 03/2016 Table 8&amp;nbsp; -- which I expected because the Android boots from the SD card.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I REALLY NEED HELP SOLVING THIS&amp;nbsp;- THANKS in ADVANCE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 21:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636882#M96991</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-20T21:01:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636883#M96992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check U-boot environment - if it is set properly for SD boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 02:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636883#M96992</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-21T02:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636884#M96993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri, &lt;/P&gt;&lt;P&gt;What does that mean? How do I check that? &lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;P&gt;Janet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 03:09:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636884#M96993</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-21T03:09:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636885#M96994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Janet,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; On the terminal, when the string "Hit any key to stop autoboot:" appears, just press any key. You will be presented with a terminal. You need to enter "printenv" command.&amp;nbsp; You need to pay more attention to "bootcmd" environment variable.&lt;/P&gt;&lt;P&gt;For further details on environment variables, you could refer to the following link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.denx.de/wiki/view/DULG/UBootEnvVariables" title="http://www.denx.de/wiki/view/DULG/UBootEnvVariables"&gt;UBootEnvVariables &amp;lt; DULG &amp;lt; DENX&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 03:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636885#M96994</guid>
      <dc:creator>Balaji_ng</dc:creator>
      <dc:date>2016-09-21T03:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636886#M96995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Balaji,&lt;/P&gt;&lt;P&gt;O.K. so here is what "printenv" shows with the u-boot.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;boot_fdt=try&lt;/P&gt;&lt;P&gt;bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimi&lt;/P&gt;&lt;P&gt;bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;/P&gt;&lt;P&gt;bootdelay=1&lt;/P&gt;&lt;P&gt;bootscript=echo Running bootscript from mmc ...; source&lt;/P&gt;&lt;P&gt;console=ttymxc0&lt;/P&gt;&lt;P&gt;emmcdev=2&lt;/P&gt;&lt;P&gt;epdc_waveform=epdc_splash.bin&lt;/P&gt;&lt;P&gt;ethact=FEC&lt;/P&gt;&lt;P&gt;ethaddr=00:04:9f:04:18:c2&lt;/P&gt;&lt;P&gt;ethprime=FEC&lt;/P&gt;&lt;P&gt;fdt_addr=0x18000000&lt;/P&gt;&lt;P&gt;fdt_file=imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;fdt_high=0xffffffff&lt;/P&gt;&lt;P&gt;image=zImage&lt;/P&gt;&lt;P&gt;initrd_addr=0x12C00000&lt;/P&gt;&lt;P&gt;initrd_high=0xffffffff&lt;/P&gt;&lt;P&gt;ip_dyn=yes&lt;/P&gt;&lt;P&gt;loadaddr=0x12000000&lt;/P&gt;&lt;P&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;/P&gt;&lt;P&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;/P&gt;&lt;P&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;/P&gt;&lt;P&gt;mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.re&lt;/P&gt;&lt;P&gt;mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}&lt;/P&gt;&lt;P&gt;mmcautodetect=yes&lt;/P&gt;&lt;P&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if;&lt;/P&gt;&lt;P&gt;mmcdev=1&lt;/P&gt;&lt;P&gt;mmcpart=1&lt;/P&gt;&lt;P&gt;mmcroot=/dev/mmcblk2p2 rootwait rw&lt;/P&gt;&lt;P&gt;netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfp&lt;/P&gt;&lt;P&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else sete;&lt;/P&gt;&lt;P&gt;script=boot.scr&lt;/P&gt;&lt;P&gt;update_emmc_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if ${gi&lt;/P&gt;&lt;P&gt;update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc di&lt;/P&gt;&lt;P&gt;　&lt;/P&gt;&lt;P&gt;Environment size: 2678/8188 bytes&lt;/P&gt;&lt;P&gt;=&amp;gt;&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;So, being new to this, how do I get this default to booting to the SD card?&amp;nbsp; I believe the variables are all ready for me so that if I booted from the "=&amp;gt;" prompt it might work, but I'm not sure of the syntax.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANKS !!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 14:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636886#M96995</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-21T14:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636887#M96996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, from looking more at the u-boot and&amp;nbsp;what&amp;nbsp;"printenv" has which is above, u-boot FIRST tries to boot from the SD card, I think, but the commands are unsuccessful so then it tries the net:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, does that mean the SD card is not correct?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;WHEN I DO THINGS MANUALLY I GET&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc dev 1&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mmc1 is current device&lt;/P&gt;&lt;P&gt;COMMENT -- this seems fine to me because /dev/sdd1 was where I saw the zImage and .dtb&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc rescan&lt;/P&gt;&lt;P&gt;=&amp;gt; fatload mmc 1:1 0x12000000 boot.src&lt;/P&gt;&lt;P&gt;reading boot.src&lt;/P&gt;&lt;P&gt;** Unable to read file boot.src **&lt;/P&gt;&lt;P&gt;COMMENT -- so here I'm in trouble !!&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt; fatload mmc 1:1 0x12000000 zImage&lt;/P&gt;&lt;P&gt;reading zImage&lt;/P&gt;&lt;P&gt;Error reading cluster&lt;/P&gt;&lt;P&gt;** Unable to read file zImage **&lt;/P&gt;&lt;P&gt;COMMENT -- so here I'm in MORE Trouble !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SO, IF I CAN SEE THE FILES ON THE SD-CARD what can cause this problem??&lt;/P&gt;&lt;P&gt;THANKS IN ADVANCE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 14:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636887#M96996</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-21T14:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636888#M96997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can also do:&lt;/P&gt;&lt;P&gt;=&amp;gt; mmc rescan&lt;/P&gt;&lt;P&gt;=&amp;gt; fatls mmc 1&lt;/P&gt;&lt;P&gt;6618968&amp;nbsp;&amp;nbsp; zimage&lt;/P&gt;&lt;P&gt;45464&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;&amp;nbsp;-- other .dtb files --&lt;/P&gt;&lt;P&gt;6 file(s), 0 dir(s)&lt;/P&gt;&lt;P&gt;=&amp;gt;&lt;/P&gt;&lt;P&gt;SO THAT LEADS ME TO BELIEVE that the "zimage" is ???&amp;nbsp;&amp;nbsp; with the Error reading cluster ???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 16:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636888#M96997</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-21T16:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636889#M96998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So,turns out that I tried 3 other SD cards and same story.&amp;nbsp; I tried a SanDisk from my QP board and it boots!&lt;/P&gt;&lt;P&gt;What's up with SD cards and u-boot?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 19:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636889#M96998</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-21T19:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636890#M96999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Janet,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; You could try to compare the partition table of your failed SD Cards with the working ones and check if you can recover any of them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, these days even I am encountering many faulty (inconsistent) SD&amp;nbsp;cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 07:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636890#M96999</guid>
      <dc:creator>Balaji_ng</dc:creator>
      <dc:date>2016-09-23T07:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636891#M97000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Balaji,&lt;/P&gt;&lt;P&gt;Thanks for the advice.&amp;nbsp; The weird thing is that on a regular PC I can see all the files.&amp;nbsp; Do you have a SD card brand that seems to be most reliable?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 23:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636891#M97000</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-23T23:28:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636892#M97001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Janet, we've just experienced similar pain flashing an image on two different 8GB Patriot SD cards, both yielding the same error as you:&lt;/P&gt;&lt;P&gt;reading zImage&lt;/P&gt;&lt;P&gt;Error reading cluster&lt;/P&gt;&lt;P&gt;After seeing your post we decided to try a 16GB Kingston and suddenly it was ok. All cards were class 10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Nov 2016 19:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636892#M97001</guid>
      <dc:creator>timlapsley</dc:creator>
      <dc:date>2016-11-23T19:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636893#M97002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also experienced a similar problem and found a solution in a &lt;A href="http://git.denx.de/?p=u-boot/u-boot-imx.git;a=commitdiff;h=58abb988ce24525474f0d515d2a36c1b3acf893f;hp=fd2d1e0d47d585eac936a7239eb2bdad7e07a8cc"&gt;commit message&lt;/A&gt; for the u-boot project from April 2016. &amp;nbsp;The text of that commit message is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;mx6ul_evk&amp;nbsp;does&amp;nbsp;not&amp;nbsp;come&amp;nbsp;with&amp;nbsp;a&amp;nbsp;eMMC&amp;nbsp;populated,&amp;nbsp;so&amp;nbsp;we&amp;nbsp;should&amp;nbsp;not&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;define&amp;nbsp;CONFIG_SUPPORT_EMMC_BOOT&amp;nbsp;as&amp;nbsp;it&amp;nbsp;causes&amp;nbsp;SPL&amp;nbsp;to&amp;nbsp;not&amp;nbsp;be&amp;nbsp;able&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;to&amp;nbsp;boot&amp;nbsp;some&amp;nbsp;brands&amp;nbsp;of&amp;nbsp;SD&amp;nbsp;cards,&amp;nbsp;such&amp;nbsp;as&amp;nbsp;SanDisk&amp;nbsp;microSD&amp;nbsp;HC&amp;nbsp;-&amp;nbsp;8GB:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;U-Boot&amp;nbsp;SPL&amp;nbsp;2016.05-rc1-28384-g108f841&amp;nbsp;(Apr&amp;nbsp;19&amp;nbsp;2016&amp;nbsp;-&amp;nbsp;11:19:11)&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;Trying&amp;nbsp;to&amp;nbsp;boot&amp;nbsp;from&amp;nbsp;MMC1&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;spl:&amp;nbsp;mmc&amp;nbsp;block&amp;nbsp;read&amp;nbsp;error&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;SPL:&amp;nbsp;failed&amp;nbsp;to&amp;nbsp;boot&amp;nbsp;from&amp;nbsp;all&amp;nbsp;boot&amp;nbsp;devices&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;###&amp;nbsp;ERROR&amp;nbsp;###&amp;nbsp;Please&amp;nbsp;RESET&amp;nbsp;the&amp;nbsp;board&amp;nbsp;###&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;When&amp;nbsp;CONFIG_SUPPORT_EMMC_BOOT&amp;nbsp;is&amp;nbsp;defined&amp;nbsp;spl_boot_mode()&amp;nbsp;returns&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;MMCSD_MODE_EMMCBOOT,&amp;nbsp;so&amp;nbsp;remove&amp;nbsp;this&amp;nbsp;option&amp;nbsp;to&amp;nbsp;have&amp;nbsp;a&amp;nbsp;reliable&amp;nbsp;boot&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;via&amp;nbsp;SD&amp;nbsp;card.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This referenced a different board than I was using, but the problem was the same. &amp;nbsp;The microSD card I experienced the problem with was a SanDisk 4GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CONFIG_SUPPORT_EMMC_BOOT is defined in /include/configs/mx6xxxxx.h in the u-boot source and is specific to your board configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 16:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636893#M97002</guid>
      <dc:creator>keno</dc:creator>
      <dc:date>2016-11-29T16:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 core-image-base-imx6qsabresd.sdcard won't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636894#M97003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi What is the last solution for this issue. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 14:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-core-image-base-imx6qsabresd-sdcard-won-t-boot/m-p/636894#M97003</guid>
      <dc:creator>sandeep_yenugul</dc:creator>
      <dc:date>2019-01-30T14:48:34Z</dc:date>
    </item>
  </channel>
</rss>