<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: EPDC Dev Boards</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635491#M96714</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1. Will the EBOOKDC4 run properly from an evk_6sl? The EBOOKDC3 was designed to work with the evk_6sl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A1. Yes, the EBOOKDC4 EPD daughter card should run properly from the i.MX6SoloLite EVK board if using the correct waveforms (the waveforms are different for the i.MX6SoloLite and i.MX7Dual processors).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. Is there a different EINK waveform/firmware file for the evk_6sl?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A2. Yes, the waveform firmware files for the same EP Display part are different for the i.MX6SoloLite EVK and i.MX7Dual SABRE SD boards, see above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. Are there epdc interface connector differences between the sabresd_7d and evk_6sl?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A3. The J12 EPD connector of the i.MX6SoloLite EVK board and the J13 EPD connector of the i.MX7Dual SABRE SD board are mostly compatible with some minor differences.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 09:34:31 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-09-29T09:34:31Z</dc:date>
    <item>
      <title>EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635490#M96713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have evk_6sl, sabresd_7d, and EBOOKDC4 devkits which are being used for the development of a product with an EINK display. The latest NXP Marshmallow release is running on both devkits. When the EBOOKDC4 is run from the sabresd_7d, the images look sharp. When the EBOOKDC4 is run from the evk_6sl, the images are blurry.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Will the EBOOKDC4 run properly from an evk_6sl? The EBOOKDC3 was designed to work with the evk_6sl.&lt;/LI&gt;&lt;LI&gt;Is there a different EINK waveform/firmware file for the evk_6sl?&lt;/LI&gt;&lt;LI&gt;Are there epdc interface connector differences between the sabresd_7d and evk_6sl?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate your help.&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 20:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635490#M96713</guid>
      <dc:creator>JohnKaye</dc:creator>
      <dc:date>2016-09-20T20:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635491#M96714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1. Will the EBOOKDC4 run properly from an evk_6sl? The EBOOKDC3 was designed to work with the evk_6sl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A1. Yes, the EBOOKDC4 EPD daughter card should run properly from the i.MX6SoloLite EVK board if using the correct waveforms (the waveforms are different for the i.MX6SoloLite and i.MX7Dual processors).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. Is there a different EINK waveform/firmware file for the evk_6sl?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A2. Yes, the waveform firmware files for the same EP Display part are different for the i.MX6SoloLite EVK and i.MX7Dual SABRE SD boards, see above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3. Are there epdc interface connector differences between the sabresd_7d and evk_6sl?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A3. The J12 EPD connector of the i.MX6SoloLite EVK board and the J13 EPD connector of the i.MX7Dual SABRE SD board are mostly compatible with some minor differences.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 09:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635491#M96714</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-09-29T09:34:31Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635492#M96715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Artur, very helpful.&lt;/P&gt;&lt;P&gt;Can you please provide, or point me at, the&amp;nbsp;EBOOKDC4 waveform files for the&amp;nbsp;i.MX6SoloLite EVK.&lt;/P&gt;&lt;P&gt;Also, I understand that there is a waveform file generation tool that NXP uses; can that be provided to me?&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 05:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635492#M96715</guid>
      <dc:creator>JohnKaye</dc:creator>
      <dc:date>2016-09-30T05:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635493#M96716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in progress of finding the correct .wbf file for the EBOOKDC4 daughter board to parse it for i.MX6SL. Will be back to youas soon as I'll find it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 11:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635493#M96716</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-10-04T11:18:24Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635494#M96717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have the default 6" EPD panel or optional 13.3" panel installed on your EBOOKDC4 daughter board? Please specify this to make me able to process the appropriate waveform file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 07:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635494#M96717</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-10-07T07:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635495#M96718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the default 6" EPD panel.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 20:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635495#M96718</guid>
      <dc:creator>JohnKaye</dc:creator>
      <dc:date>2016-10-07T20:25:13Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635496#M96719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;Any progress on the waveform file?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2016 15:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635496#M96719</guid>
      <dc:creator>JohnKaye</dc:creator>
      <dc:date>2016-10-11T15:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: EPDC Dev Boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635497#M96720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try both of the attached ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 10:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EPDC-Dev-Boards/m-p/635497#M96720</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-10-18T10:10:44Z</dc:date>
    </item>
  </channel>
</rss>