<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IOMUX Configuration For IPU1 in IMX6DQ in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IOMUX-Configuration-For-IPU1-in-IMX6DQ/m-p/635044#M96613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am doing some bare-metal programming in iMX6DQ SABRE-SD board. I am using UART1 as the debug serial port. While configuring my UART i have set the&amp;nbsp;Pad Mux Register(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA10) mux mode field as "011". However, When i try to configure the IPU1 for the device, i have the set the mux mode as "000", as i have observed from the "1.1.0_iMX6_Platform_SDK".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use both these modules simultaneously?&amp;nbsp;&lt;/P&gt;&lt;P&gt;or should i go for IPU2?&lt;/P&gt;&lt;P&gt;I have never worked with IPU at this level before. Please Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ajmal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Mar 2017 11:56:27 GMT</pubDate>
    <dc:creator>ajmalali</dc:creator>
    <dc:date>2017-03-31T11:56:27Z</dc:date>
    <item>
      <title>IOMUX Configuration For IPU1 in IMX6DQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IOMUX-Configuration-For-IPU1-in-IMX6DQ/m-p/635044#M96613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am doing some bare-metal programming in iMX6DQ SABRE-SD board. I am using UART1 as the debug serial port. While configuring my UART i have set the&amp;nbsp;Pad Mux Register(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA10) mux mode field as "011". However, When i try to configure the IPU1 for the device, i have the set the mux mode as "000", as i have observed from the "1.1.0_iMX6_Platform_SDK".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use both these modules simultaneously?&amp;nbsp;&lt;/P&gt;&lt;P&gt;or should i go for IPU2?&lt;/P&gt;&lt;P&gt;I have never worked with IPU at this level before. Please Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ajmal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 11:56:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IOMUX-Configuration-For-IPU1-in-IMX6DQ/m-p/635044#M96613</guid>
      <dc:creator>ajmalali</dc:creator>
      <dc:date>2017-03-31T11:56:27Z</dc:date>
    </item>
    <item>
      <title>Re: IOMUX Configuration For IPU1 in IMX6DQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IOMUX-Configuration-For-IPU1-in-IMX6DQ/m-p/635045#M96614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ajmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately there is no way to use simultaneously gpio and lcd(ipu),&lt;/P&gt;&lt;P&gt;so it is necessary to reassign signal to other pad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 23:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IOMUX-Configuration-For-IPU1-in-IMX6DQ/m-p/635045#M96614</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-31T23:38:39Z</dc:date>
    </item>
  </channel>
</rss>