<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Adding a non-supported imx6 BSP layer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-a-non-supported-imx6-BSP-layer/m-p/634207#M96521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yvon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is necessary to create your custom-machine.conf file and put it inside meta-fsl-arm/conf/machine folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the tool you are using is not manufactured by NXP, so for further information about creating .conf file please contact Armadeus Systems.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Mar 2017 16:38:42 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-03-08T16:38:42Z</dc:date>
    <item>
      <title>Adding a non-supported imx6 BSP layer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-a-non-supported-imx6-BSP-layer/m-p/634206#M96520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I aim to build a linux-imx for an Armadeus iMX6 machine (apf6dev_dual), in the BSP Linux 4.1.15_1.2.0 environment (note: while not supported by the FSL Community BSP, Armadeus boards are in the kernel mainline).&lt;/P&gt;&lt;P&gt;Armadeus provides a Yocto BSP layer for its boards, but it has not yet been used in a NXP BSP build environment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So after initializing the fsl-arm-yocto-bsp with &lt;SPAN style="font-family: andale mono,monospace;"&gt;&lt;STRONG&gt;repo&lt;/STRONG&gt;&lt;/SPAN&gt;, I downloaded and unzipped the &lt;A href="https://github.com/trabucayre/meta-armadeus/tree/krogoth"&gt;meta-armadeus BSP&lt;/A&gt; (krogoth branch) within the "&lt;STRONG style="font-family: andale mono,monospace;"&gt;sources&lt;/STRONG&gt;" sub-directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Freescale Yocto Project User's Guide ("8 Creating a Custom Board Configuration"), the next step is to run the command "&lt;SPAN style="font-family: andale mono,monospace;"&gt;&lt;STRONG&gt;source setup-environment build&lt;/STRONG&gt;&lt;/SPAN&gt;". However this command sets up an environment for the default "&lt;STRONG style="font-family: andale mono,monospace;"&gt;imx6qsabresd&lt;/STRONG&gt;" machine. So i tried instead with the command "&lt;SPAN style="font-family: andale mono,monospace;"&gt;&lt;STRONG&gt;MACHINE=apf6dev-dual DISTRO=fsl-imx-fb source ./fsl-setup-release.sh -b build&lt;/STRONG&gt;&lt;/SPAN&gt;"... but I got the message :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="font-family: andale mono,monospace;"&gt;The $MACHINE you have specified (apf6dev-dual) is not supported by this build setup&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1 : Is is possible/allowed to build a machine of a BSP not supported by the FSL Community BSP ?&lt;/P&gt;&lt;P&gt;Q2 : If it is, how to set up the environment so that this machine is taken into account by the NXP BSP environment ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help,&lt;/P&gt;&lt;P&gt;-Yvon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 14:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-a-non-supported-imx6-BSP-layer/m-p/634206#M96520</guid>
      <dc:creator>yvongrall</dc:creator>
      <dc:date>2017-03-08T14:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a non-supported imx6 BSP layer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-a-non-supported-imx6-BSP-layer/m-p/634207#M96521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yvon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is necessary to create your custom-machine.conf file and put it inside meta-fsl-arm/conf/machine folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the tool you are using is not manufactured by NXP, so for further information about creating .conf file please contact Armadeus Systems.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 16:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-a-non-supported-imx6-BSP-layer/m-p/634207#M96521</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-03-08T16:38:42Z</dc:date>
    </item>
  </channel>
</rss>