<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: bitbake recipe make: *** No rule to make target `install' in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634199#M96519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My system is Ubuntu 14.04, I will try with bitbake&amp;nbsp; -c cleanall . this is my configuration file&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;MACHINE ??= 'test-dual'&lt;BR /&gt;DISTRO ?= 'poky'&lt;BR /&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;BR /&gt;EXTRA_IMAGE_FEATURES = "debug-tweaks"&lt;BR /&gt;USER_CLASSES ?= "buildstats image-mklibs image-prelink"&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;BR /&gt;BB_DISKMON_DIRS = "\&lt;BR /&gt; STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt; STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt; ABORT,${TMPDIR},100M,1K \&lt;BR /&gt; ABORT,${DL_DIR},100M,1K \&lt;BR /&gt; ABORT,${SSTATE_DIR},100M,1K" &lt;BR /&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;BR /&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;BR /&gt;ASSUME_PROVIDED += "libsdl-native"&lt;BR /&gt;CONF_VERSION = "1"&lt;BR /&gt;BB_NUMBER_THREADS = '4'&lt;BR /&gt;PARALLEL_MAKE = '-j 4'&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;BR /&gt;ACCEPT_FSL_EULA = ""&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jan 2017 02:39:16 GMT</pubDate>
    <dc:creator>anjojohn</dc:creator>
    <dc:date>2017-01-31T02:39:16Z</dc:date>
    <item>
      <title>bitbake recipe make: *** No rule to make target `install'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634197#M96517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have a recipe file for libre. In yocto 1.6.1 its successfully installed. But in yocto 1.8.1 its failing with make: *** No rule to make target `install'. below is the recipe file for libre&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PROVIDES_${PN} = "re"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SRC_URI = "&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcreytiv.com%2Fpub%2Fre-0.4.17.tar.gz" rel="nofollow" target="_blank"&gt;http://creytiv.com/pub/re-0.4.17.tar.gz&lt;/A&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;BR /&gt;SRC_URI[md5sum] = "5900337fd8c77515c87eae5bf0f8c091"&lt;BR /&gt;SRC_URI[sha256sum] = "2ce089b64909dc2aaa71421245e3a76dfe8a3279478f3eebd2aaead591106098"&lt;BR /&gt;inherit autotools&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DEPENDS = "openssl zlib"&lt;BR /&gt;FILES_{PN} += "${libdir}/*"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure why oe_runmake is not able to find the make file.&lt;/P&gt;&lt;P&gt;below is the debug&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_install&lt;BR /&gt;| NOTE: make -j 4 DESTDIR=/home/anjo/eliu_accs/eliu_accs/src/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/re/0.4.17-r0/image install&lt;BR /&gt;| make: *** No rule to make target `install'.&amp;nbsp; Stop.&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_install (log file is located at /home/anjo/eliu_accs/eliu_accs/src/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/re/0.4.17-r0/temp/log.do_install.6041)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 10:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634197#M96517</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-01-20T10:44:15Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake recipe make: *** No rule to make target `install'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634198#M96518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi anjo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is your linux host?&amp;nbsp;I would recommend using Ubuntu 14.04 if at all possible,&amp;nbsp;as NXP BSP Release dependencies may be different in newer Ubuntu releases. It should be possible to look for the equivalent host packages but I haven’t tried it myself. (The core-image-minimal uses only packages from the Yocto Project, so it is possible that the dependencies for the Yocto Project are met but not for the NXP BSP Release layers)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have seen any error in your description, just you need to share your conf file.&lt;/P&gt;&lt;P&gt;try with bitbake c-c cleanall and restart the process&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 00:24:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634198#M96518</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2017-01-31T00:24:45Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake recipe make: *** No rule to make target `install'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634199#M96519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My system is Ubuntu 14.04, I will try with bitbake&amp;nbsp; -c cleanall . this is my configuration file&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;MACHINE ??= 'test-dual'&lt;BR /&gt;DISTRO ?= 'poky'&lt;BR /&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;BR /&gt;EXTRA_IMAGE_FEATURES = "debug-tweaks"&lt;BR /&gt;USER_CLASSES ?= "buildstats image-mklibs image-prelink"&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;BR /&gt;BB_DISKMON_DIRS = "\&lt;BR /&gt; STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt; STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt; ABORT,${TMPDIR},100M,1K \&lt;BR /&gt; ABORT,${DL_DIR},100M,1K \&lt;BR /&gt; ABORT,${SSTATE_DIR},100M,1K" &lt;BR /&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;BR /&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;BR /&gt;ASSUME_PROVIDED += "libsdl-native"&lt;BR /&gt;CONF_VERSION = "1"&lt;BR /&gt;BB_NUMBER_THREADS = '4'&lt;BR /&gt;PARALLEL_MAKE = '-j 4'&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;BR /&gt;ACCEPT_FSL_EULA = ""&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 02:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-recipe-make-No-rule-to-make-target-install/m-p/634199#M96519</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-01-31T02:39:16Z</dc:date>
    </item>
  </channel>
</rss>