<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックU-Boot initializing failure</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-initializing-failure/m-p/190976#M9636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For a week or so I work with the i.MX53 QSB. In this time I've managed to start up both a Linux Gnome build and Windows Compact 7 on the QSB via uSD. Only today I've failed to start up the Linux builds of the FSL orginal uSD with Ubuntu as well as my own Linux Gnome build.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to start up Linux, the QSB won't give any output to the serial console and won't start the start-up sequence. However, when I try to start up Windows Compact 7, all works fine.&lt;/P&gt;&lt;P&gt;Because I get no serial feedback from the QSB, I think it's safe to assume that the problem is caused by U-boot..? Or is there anything else I should know about the prebootloader that can cause this problem.&lt;/P&gt;&lt;P&gt;Please, can anyone help with finding the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Nov 2011 10:27:25 GMT</pubDate>
    <dc:creator>JosSchuts</dc:creator>
    <dc:date>2011-11-24T10:27:25Z</dc:date>
    <item>
      <title>U-Boot initializing failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-initializing-failure/m-p/190976#M9636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For a week or so I work with the i.MX53 QSB. In this time I've managed to start up both a Linux Gnome build and Windows Compact 7 on the QSB via uSD. Only today I've failed to start up the Linux builds of the FSL orginal uSD with Ubuntu as well as my own Linux Gnome build.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to start up Linux, the QSB won't give any output to the serial console and won't start the start-up sequence. However, when I try to start up Windows Compact 7, all works fine.&lt;/P&gt;&lt;P&gt;Because I get no serial feedback from the QSB, I think it's safe to assume that the problem is caused by U-boot..? Or is there anything else I should know about the prebootloader that can cause this problem.&lt;/P&gt;&lt;P&gt;Please, can anyone help with finding the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2011 10:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-initializing-failure/m-p/190976#M9636</guid>
      <dc:creator>JosSchuts</dc:creator>
      <dc:date>2011-11-24T10:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot initializing failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-initializing-failure/m-p/190977#M9637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where is the prebootloader for WINCE boot placed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2011 16:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-initializing-failure/m-p/190977#M9637</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2011-11-29T16:05:01Z</dc:date>
    </item>
  </channel>
</rss>