<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to achieve  Scalar functionality dynamically on imx6? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-achieve-Scalar-functionality-dynamically-on-imx6/m-p/633287#M96316</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Scalar support tested:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have checked the scaling by converting the low resolution image (.bmp or any format) to raw data by referring&amp;nbsp;&amp;nbsp;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-94961" title="https://community.freescale.com/docs/DOC-94961"&gt;ipu-examples release notes - v0.1 | NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then up-scaled the raw data to higher resolution(say 1920*1080) using IPU and dumped(up-scaled raw data) on respective high resolution LVDS display.&lt;BR /&gt;Raw data now fits properly on the Full HD display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Query:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the query is we will be doing multiple activities in time, and is it possible to achieve the scaling dynamically??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Consider the Frame buffer size to 800*480 and the display connected is 1920*1080&amp;nbsp; to the processor (Not sure whether we can configure like this).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12909iDC8CEFEE9FD3A1E1/image-size/large?v=v2&amp;amp;px=999" title="scalar.png" alt="scalar.png" /&gt;&lt;/span&gt;&lt;BR /&gt;When with the above setup, contents frame buffer should be scaled using internal scalar of the processor to 1920*1080 and dump on FHD display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any procedure do the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ambika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jan 2017 06:21:22 GMT</pubDate>
    <dc:creator>ambika</dc:creator>
    <dc:date>2017-01-20T06:21:22Z</dc:date>
    <item>
      <title>How to achieve  Scalar functionality dynamically on imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-achieve-Scalar-functionality-dynamically-on-imx6/m-p/633287#M96316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Scalar support tested:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have checked the scaling by converting the low resolution image (.bmp or any format) to raw data by referring&amp;nbsp;&amp;nbsp;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-94961" title="https://community.freescale.com/docs/DOC-94961"&gt;ipu-examples release notes - v0.1 | NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then up-scaled the raw data to higher resolution(say 1920*1080) using IPU and dumped(up-scaled raw data) on respective high resolution LVDS display.&lt;BR /&gt;Raw data now fits properly on the Full HD display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Query:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the query is we will be doing multiple activities in time, and is it possible to achieve the scaling dynamically??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Consider the Frame buffer size to 800*480 and the display connected is 1920*1080&amp;nbsp; to the processor (Not sure whether we can configure like this).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12909iDC8CEFEE9FD3A1E1/image-size/large?v=v2&amp;amp;px=999" title="scalar.png" alt="scalar.png" /&gt;&lt;/span&gt;&lt;BR /&gt;When with the above setup, contents frame buffer should be scaled using internal scalar of the processor to 1920*1080 and dump on FHD display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any procedure do the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ambika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 06:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-achieve-Scalar-functionality-dynamically-on-imx6/m-p/633287#M96316</guid>
      <dc:creator>ambika</dc:creator>
      <dc:date>2017-01-20T06:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to achieve  Scalar functionality dynamically on imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-achieve-Scalar-functionality-dynamically-on-imx6/m-p/633288#M96317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="252308" data-username="ambika@iwavesystems.com" href="https://community.nxp.com/people/ambika@iwavesystems.com"&gt;Ambika&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp; For i.mx6,&amp;nbsp; scaling single picture is no problem, but it doesn't support your scaling application.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jan 2017 10:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-achieve-Scalar-functionality-dynamically-on-imx6/m-p/633288#M96317</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-01-22T10:29:43Z</dc:date>
    </item>
  </channel>
</rss>