<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Multiple WiFi interfaces in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-WiFi-interfaces/m-p/633050#M96289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got custom boards that need to support wireless Ethernet either via an on-board wireless module or through a USB wireless interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything works as I expect when only one of the interfaces is present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I boot the board with the on-board wireless module and a USB wireless interface attached the on-board module is loaded as wlan1 and the USB interface is loaded as wlan0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really want to have the on-board module always identify as wlan0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas on what I need to change to always force the on-board module to load as wlan0 if it is present?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our kernel is based on Marshmallow (git tag android-6.0.1_r22), kernel 4.1.15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;&amp;nbsp; Peter Steinberg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Feb 2017 22:19:10 GMT</pubDate>
    <dc:creator>petersteinberg</dc:creator>
    <dc:date>2017-02-14T22:19:10Z</dc:date>
    <item>
      <title>Multiple WiFi interfaces</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-WiFi-interfaces/m-p/633050#M96289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got custom boards that need to support wireless Ethernet either via an on-board wireless module or through a USB wireless interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything works as I expect when only one of the interfaces is present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I boot the board with the on-board wireless module and a USB wireless interface attached the on-board module is loaded as wlan1 and the USB interface is loaded as wlan0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really want to have the on-board module always identify as wlan0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas on what I need to change to always force the on-board module to load as wlan0 if it is present?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our kernel is based on Marshmallow (git tag android-6.0.1_r22), kernel 4.1.15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;&amp;nbsp; Peter Steinberg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 22:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-WiFi-interfaces/m-p/633050#M96289</guid>
      <dc:creator>petersteinberg</dc:creator>
      <dc:date>2017-02-14T22:19:10Z</dc:date>
    </item>
  </channel>
</rss>