<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx25 SRAM CS0 configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx25-SRAM-CS0-configuration/m-p/190942#M9628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems to be a easy configuration but i cannot make it work.&lt;/P&gt;&lt;P&gt;I tring to configure the cs0 area to access an external 16 bit peripheral that works as a asyncornous memory. (it has also a wait# signal)&lt;/P&gt;&lt;P&gt;SO i configured the&lt;/P&gt;&lt;P&gt;Chip Select 0 Upper Control Register 0x00000787&lt;BR /&gt; Chip Select 0 Lower Control Register 0x00000D01&lt;BR /&gt;Chip Select 0 Additional Control Register 0x00000000&lt;/P&gt;&lt;P&gt;accessing it using a LDR istruction (writing and reading it) (32 bit access) i should have two write access (EB0 and eb1 goes low 2 time ) and during reding i should see oe goes low 2 tiems as well (accordly with the timing digrams on the ref manual).&lt;/P&gt;&lt;P&gt;but i have a very strange behaviour... first of all i can see just one access in wr or in read...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;then i tried to add some setup and holt time ( OEA != 0 in the lower control reg)... well now i see O goes low several times .. even 16 time for each acces.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm doing something very wrong... but what...&lt;/P&gt;&lt;P&gt;it should be a very simple set up...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i did another test and i noticed.&lt;/P&gt;&lt;P&gt;one more strange bahaviour, the access time during a write is related to the WSC i set (I disabled the WAIT in this test) but the read access time is much more longer.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Nov 2011 13:18:03 GMT</pubDate>
    <dc:creator>OmarPighi</dc:creator>
    <dc:date>2011-11-24T13:18:03Z</dc:date>
    <item>
      <title>imx25 SRAM CS0 configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx25-SRAM-CS0-configuration/m-p/190942#M9628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems to be a easy configuration but i cannot make it work.&lt;/P&gt;&lt;P&gt;I tring to configure the cs0 area to access an external 16 bit peripheral that works as a asyncornous memory. (it has also a wait# signal)&lt;/P&gt;&lt;P&gt;SO i configured the&lt;/P&gt;&lt;P&gt;Chip Select 0 Upper Control Register 0x00000787&lt;BR /&gt; Chip Select 0 Lower Control Register 0x00000D01&lt;BR /&gt;Chip Select 0 Additional Control Register 0x00000000&lt;/P&gt;&lt;P&gt;accessing it using a LDR istruction (writing and reading it) (32 bit access) i should have two write access (EB0 and eb1 goes low 2 time ) and during reding i should see oe goes low 2 tiems as well (accordly with the timing digrams on the ref manual).&lt;/P&gt;&lt;P&gt;but i have a very strange behaviour... first of all i can see just one access in wr or in read...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;then i tried to add some setup and holt time ( OEA != 0 in the lower control reg)... well now i see O goes low several times .. even 16 time for each acces.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm doing something very wrong... but what...&lt;/P&gt;&lt;P&gt;it should be a very simple set up...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i did another test and i noticed.&lt;/P&gt;&lt;P&gt;one more strange bahaviour, the access time during a write is related to the WSC i set (I disabled the WAIT in this test) but the read access time is much more longer.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2011 13:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx25-SRAM-CS0-configuration/m-p/190942#M9628</guid>
      <dc:creator>OmarPighi</dc:creator>
      <dc:date>2011-11-24T13:18:03Z</dc:date>
    </item>
  </channel>
</rss>