<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Diagnose Mfgtool Bad Data CRC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632982#M96271</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor&lt;BR /&gt;Thanks for your suggestion, but CONFIG_BLK_DEV_RAM_SIZE affects the Kernel. My problem is seen in U-boot.&lt;BR /&gt;For example, if I get the mfgtool to load the rootfs twice into RAM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="BootStrap" type="load" file="firmware/fsl-image-mfgtool-initramfs.cpio.gz.u-boot" address="0x12C00000"&lt;BR /&gt;loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q"&amp;gt;Loading Initramfs1.&amp;lt;/CMD&amp;gt;&lt;BR /&gt;&amp;lt;CMD state="BootStrap" type="load" file="firmware/fsl-image-mfgtool-initramfs.cpio.gz.u-boot" address="0x20000000"&lt;BR /&gt;loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q"&amp;gt;Loading Initramfs2.&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then compare the two data blocks:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cmp.b 0x12C00000 0x20000000 5000000&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; cmp.b 0x12C00000 0x20000000 5000000&lt;BR /&gt;byte at 0x13963680 (0x21) != byte at 0x20d63680 (0xbe)&lt;BR /&gt;Total of 14038656 byte(s) were the same&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The location of the difference will change every time I load the data over USB, and sometimes the data matches!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jan 2017 09:43:16 GMT</pubDate>
    <dc:creator>simonr99</dc:creator>
    <dc:date>2017-01-25T09:43:16Z</dc:date>
    <item>
      <title>Diagnose Mfgtool Bad Data CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632980#M96269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm setting up Mfgtool re-flashing of my Hummingboard i.MX6Q system. I've built a mfgtool U-boot, kernel and rootfs using Yocto.&lt;/P&gt;&lt;P&gt;When I boot over OTG USB using Mfgtool my target &lt;STRONG&gt;&lt;EM&gt;sometimes&lt;/EM&gt; &lt;/STRONG&gt;successfully boots into the linux kernel. Most attempts fail with:&lt;/P&gt;&lt;PRE class="" style="color: #333333; background-color: #f5f5f5; font-size: 12px;"&gt;## Loading init Ramdisk from Legacy Image at 12c00000 ...&amp;nbsp;&amp;nbsp;&amp;nbsp; 
Image Name:&amp;nbsp;&amp;nbsp; fsl-image-mfgtool-initramfs-soli&amp;nbsp;&amp;nbsp;&amp;nbsp; 
Image Type:&amp;nbsp;&amp;nbsp; ARM Linux RAMDisk Image (gzip compressed)&amp;nbsp;&amp;nbsp;&amp;nbsp; 
Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 88443107 Bytes = 84.3 MiB&amp;nbsp;&amp;nbsp;&amp;nbsp; 
Load Address: 00000000&amp;nbsp;&amp;nbsp;&amp;nbsp; 
Entry Point:&amp;nbsp; 00000000&amp;nbsp;&amp;nbsp;&amp;nbsp; 
Verifying Checksum ... Bad Data CRC 
Ramdisk image is corrupt or invalid&lt;/PRE&gt;&lt;P&gt;Because of the intermittent nature of the failure I suspected DDR calibration problems. So I've run the DDR Stress Tester with the settings used by my Mfgtool U-boot. The stress test passed without needing calibration data changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I modify my ucl2.xml to load the initramfs file into memory twice in different locations, and then run cmp in U-boot, the data is different. Run cmp again and I get the same difference. So the error occurred during the write to RAM, not the read.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I do a cp in u-boot to copy a large block of data and then a cmp to compare the memory areas, they are the same.&lt;/P&gt;&lt;P&gt;Can I then conclude that my errors occur during USB data transfer?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone suggest how to diagnose further, or what could be the problem?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 09:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632980#M96269</guid>
      <dc:creator>simonr99</dc:creator>
      <dc:date>2017-01-20T09:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: Diagnose Mfgtool Bad Data CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632981#M96270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Simon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to decrease image size or check imx_v7_mfg_defconfig &lt;BR /&gt;CONFIG_BLK_DEV_RAM_SIZE mentioned in &lt;BR /&gt;&lt;A href="http://stackoverflow.com/questions/36387516/size-constraints-of-initramfs-on-arm"&gt;http://stackoverflow.com/questions/36387516/size-constraints-of-initramfs-on-arm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 23:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632981#M96270</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-20T23:10:18Z</dc:date>
    </item>
    <item>
      <title>Re: Diagnose Mfgtool Bad Data CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632982#M96271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor&lt;BR /&gt;Thanks for your suggestion, but CONFIG_BLK_DEV_RAM_SIZE affects the Kernel. My problem is seen in U-boot.&lt;BR /&gt;For example, if I get the mfgtool to load the rootfs twice into RAM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="BootStrap" type="load" file="firmware/fsl-image-mfgtool-initramfs.cpio.gz.u-boot" address="0x12C00000"&lt;BR /&gt;loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q"&amp;gt;Loading Initramfs1.&amp;lt;/CMD&amp;gt;&lt;BR /&gt;&amp;lt;CMD state="BootStrap" type="load" file="firmware/fsl-image-mfgtool-initramfs.cpio.gz.u-boot" address="0x20000000"&lt;BR /&gt;loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q"&amp;gt;Loading Initramfs2.&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then compare the two data blocks:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cmp.b 0x12C00000 0x20000000 5000000&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; cmp.b 0x12C00000 0x20000000 5000000&lt;BR /&gt;byte at 0x13963680 (0x21) != byte at 0x20d63680 (0xbe)&lt;BR /&gt;Total of 14038656 byte(s) were the same&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The location of the difference will change every time I load the data over USB, and sometimes the data matches!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 09:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632982#M96271</guid>
      <dc:creator>simonr99</dc:creator>
      <dc:date>2017-01-25T09:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: Diagnose Mfgtool Bad Data CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632983#M96272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Simon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you try to load some small (&amp;lt;1MB) binary file with patterns (like all zeros, all "1", e.t.c)&lt;/P&gt;&lt;P&gt;instead fsl-image-mfgtool-initramfs.cpio.gz and check it. If difference persist this may point to&lt;/P&gt;&lt;P&gt;ddr errors or board supply issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 09:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632983#M96272</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-25T09:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: Diagnose Mfgtool Bad Data CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632984#M96273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried loading files of different sizes and investigating the error rate. An 8Mbyte file will nearly always load correctly. An 80Mbyte nearly always gets corrupted.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I then realised that my mfgtool-initramfs file is far larger than average (80MBytes - the examples are &amp;lt; 8MBytes) and so I fixed this in my Yocto layers (caused by specifying packages globally in local.conf).&lt;/P&gt;&lt;P&gt;My mfgtool-initramfs is now 7MBytes, so usually loads without errors. This is a work-around rather than a fix - there is still an error rate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 11:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Diagnose-Mfgtool-Bad-Data-CRC/m-p/632984#M96273</guid>
      <dc:creator>simonr99</dc:creator>
      <dc:date>2017-01-26T11:52:50Z</dc:date>
    </item>
  </channel>
</rss>