<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MX7SABRE Boot Config Settings</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632748#M96235</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your comments. As I said above, we already did the resistor adjustments (OK, we could not locate R398 on the PCB, but QSPIA_SS1_B is not used so I think this has no effect). Otherwise, we would not be able to read and write the QSPI flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There must be another problem with boot configuration settings. We have a second i.MX7 SABRE board here with no resistor modifications. I understand that fuses are burnt to boot from SD card, but when SW3 is switched to [01]&amp;nbsp; (serial download mode) the board still boots from SD card plugged in. It is not possible to boot via serial download mode then. Serial download mode will only work when SD card is removed from the slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe this is a mistake because it is not possible to boot the board in case that a broken bootloader is stored in the boot device that cannot be remove, e.g. a QSPI flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you explain what happens here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Mar 2017 08:59:06 GMT</pubDate>
    <dc:creator>thomasschaefer</dc:creator>
    <dc:date>2017-03-30T08:59:06Z</dc:date>
    <item>
      <title>MX7SABRE Boot Config Settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632746#M96233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to boot our i.MX7 SABRE board from the onboard QSPI flash. I managed to activate the flash by reworking resistors as described in the QSPI NOR Flash section of the schematics. When booting via Serial Downloader, I can load and write bootloader binary image into QSPI flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the board does not boot from the QSPI device. I have removed the supplied SD card containing original u-boot and set BOOT_MODE switch SW3 to [10] (internal boot) and boot config switch SW2 to [10000000] as shown in schematics and printing on the board. It is only possible to load u-boot via serial download mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even more, if SD card is attached, the board only boots from SD card, it is not possible to boot from serial downloader or QSPI flash. This is independent from Boot Config (SW2) and BOOT_MODE (SW3) settings with the exception that the board won't boot anymore if BOOT_MODE is set to [11] (Test Mode), but that's OK I think.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do to manage booting from QSPI flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 15:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632746#M96233</guid>
      <dc:creator>thomasschaefer</dc:creator>
      <dc:date>2017-03-29T15:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: MX7SABRE Boot Config Settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632747#M96234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="269003" data-username="thomasschaefer" href="https://community.nxp.com/people/thomasschaefer"&gt;Thomas &lt;/A&gt;，&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;set BOOT_MODE switch SW3 to [10] (internal boot) and boot config switch SW2 to [10000000]&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your settings are correct.&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;See page 9 of schematic with PDF format&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16275i1F8B7CF8F5DD3293/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Some resistors should also be adjusted on MX7Sabre Board!&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 03:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632747#M96234</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-03-30T03:06:14Z</dc:date>
    </item>
    <item>
      <title>Re: MX7SABRE Boot Config Settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632748#M96235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your comments. As I said above, we already did the resistor adjustments (OK, we could not locate R398 on the PCB, but QSPIA_SS1_B is not used so I think this has no effect). Otherwise, we would not be able to read and write the QSPI flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There must be another problem with boot configuration settings. We have a second i.MX7 SABRE board here with no resistor modifications. I understand that fuses are burnt to boot from SD card, but when SW3 is switched to [01]&amp;nbsp; (serial download mode) the board still boots from SD card plugged in. It is not possible to boot via serial download mode then. Serial download mode will only work when SD card is removed from the slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe this is a mistake because it is not possible to boot the board in case that a broken bootloader is stored in the boot device that cannot be remove, e.g. a QSPI flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you explain what happens here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 08:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632748#M96235</guid>
      <dc:creator>thomasschaefer</dc:creator>
      <dc:date>2017-03-30T08:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: MX7SABRE Boot Config Settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632749#M96236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking further into this I found the description of the SD/MMC Manufacture Mode:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SD_MMC_ManufactureBootFlow.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17512i0C5C675B706CC775/image-size/large?v=v2&amp;amp;px=999" role="button" title="SD_MMC_ManufactureBootFlow.PNG" alt="SD_MMC_ManufactureBootFlow.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At least, I understand now why serial downloader is overridden when BOOT_MODE is set to 01b - the SDMMC MFG mode is not disabled on our board. Will try to find out why internal boot (BOOT_MODE = 10b) from QSPI fails now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 09:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632749#M96236</guid>
      <dc:creator>thomasschaefer</dc:creator>
      <dc:date>2017-03-31T09:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: MX7SABRE Boot Config Settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632750#M96237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally I've learned that booting from QSPI requires a set of configuration parameters (see chapter 6.6.6.3 of the RM) stored in the flash device from offset 0x0 on (the RM Rev 0.1 states that configuration parameters are stored at offset 0x400, but this is wrong as here is the location for the bootloader binary image).&lt;/P&gt;&lt;P&gt;The MFGTOOL contains the configuration parameters for different QSPI devices and with that I was able to create a 512 byte binary blob and write it into the QSPI device at offset 0x0. Now I can boot the MX7SABRE from QSPI flash with bootloader stored at offset 0x400.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are my steps to create the configuration parameter binary blob (&lt;STRONG&gt;qspi-header.sh&lt;/STRONG&gt; and &lt;STRONG&gt;qspi-nor-macronix-mx25l51245g-config&lt;/STRONG&gt; are from the MFGTOOL package):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;# Create QSPI header ASCII file (qspi-tmp)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;# sh qspi-header.sh qspi-nor-macronix-mx25l51245g-config&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;#&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;# Create QSPI configuration header binary blob&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier,monospace;"&gt;# cat qspi-tmp | xxd -r &amp;gt;qspi-header.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 12:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7SABRE-Boot-Config-Settings/m-p/632750#M96237</guid>
      <dc:creator>thomasschaefer</dc:creator>
      <dc:date>2017-04-03T12:26:47Z</dc:date>
    </item>
  </channel>
</rss>