<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: point cloud library @ yocto imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/point-cloud-library-yocto-imx6/m-p/632056#M96106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erik Raynolds,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Point Cloud Library is part of the ROS project. There is a meta-ros layer that contains support for this software but you would need to add the layer manually to the Release BSP as it’s not included.&lt;/P&gt;&lt;P&gt;You may find information on this on the following page:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://layers.openembedded.org/layerindex/recipe/23141/"&gt;https://layers.openembedded.org/layerindex/recipe/23141/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Oct 2016 20:47:55 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-10-13T20:47:55Z</dc:date>
    <item>
      <title>point cloud library @ yocto imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/point-cloud-library-yocto-imx6/m-p/632055#M96105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there recipes for "Point Cloud Library" for yocto image build?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 09:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/point-cloud-library-yocto-imx6/m-p/632055#M96105</guid>
      <dc:creator>erikraynolds</dc:creator>
      <dc:date>2016-10-13T09:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: point cloud library @ yocto imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/point-cloud-library-yocto-imx6/m-p/632056#M96106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erik Raynolds,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Point Cloud Library is part of the ROS project. There is a meta-ros layer that contains support for this software but you would need to add the layer manually to the Release BSP as it’s not included.&lt;/P&gt;&lt;P&gt;You may find information on this on the following page:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://layers.openembedded.org/layerindex/recipe/23141/"&gt;https://layers.openembedded.org/layerindex/recipe/23141/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 20:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/point-cloud-library-yocto-imx6/m-p/632056#M96106</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-10-13T20:47:55Z</dc:date>
    </item>
  </channel>
</rss>