<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to format eMMC using U-boot in imx6? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-format-eMMC-using-U-boot-in-imx6/m-p/632039#M96097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a custom board with imx6. I am trying to use the fastboot on the eMMC to flash the MBR table but it works only if the eMMC has gpt format.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to partition the eMMC for the first time if it is mounted on the board already.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Dec 2016 12:18:29 GMT</pubDate>
    <dc:creator>hishamelmeligi</dc:creator>
    <dc:date>2016-12-21T12:18:29Z</dc:date>
    <item>
      <title>How to format eMMC using U-boot in imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-format-eMMC-using-U-boot-in-imx6/m-p/632039#M96097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a custom board with imx6. I am trying to use the fastboot on the eMMC to flash the MBR table but it works only if the eMMC has gpt format.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to partition the eMMC for the first time if it is mounted on the board already.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2016 12:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-format-eMMC-using-U-boot-in-imx6/m-p/632039#M96097</guid>
      <dc:creator>hishamelmeligi</dc:creator>
      <dc:date>2016-12-21T12:18:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to format eMMC using U-boot in imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-format-eMMC-using-U-boot-in-imx6/m-p/632040#M96098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hisham&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to programming emmc with uboot (Warp7 board)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.denx.de/?p=u-boot.git;a=blob;f=board/warp7/README;h=60339da543732829d4ac09f02178cb84dfa3b1ad;hb=HEAD"&gt;http://git.denx.de/?p=u-boot.git;a=blob;f=board/warp7/README;h=60339da543732829d4ac09f02178cb84dfa3b1ad;hb=HEAD&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 11:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-format-eMMC-using-U-boot-in-imx6/m-p/632040#M96098</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-29T11:29:55Z</dc:date>
    </item>
  </channel>
</rss>