<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Yocto build error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-build-error/m-p/631544#M96024</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erik Raynolds,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that this recipe, which is part of Open Embedded, is broken and the repository where the source was it-s no longer there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the following bug:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.yoctoproject.org/bug/bug-8253-vim-recipe-broken"&gt;https://www.yoctoproject.org/bug/bug-8253-vim-recipe-broken&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that the BSP Release you are using refers to a specific commit in the past unlike the Community BSP which is constantly changing. My recommendation would be switching to the 4.1.15 BSP Release to see if the recipe is fixed there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another alternative would be looking for the new repository for this recipe and manually fixing it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Flayers.openembedded.org%2Flayerindex%2Frecipe%2F5559%2F" rel="nofollow" target="_blank"&gt;https://layers.openembedded.org/layerindex/recipe/5559/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Oct 2016 20:30:54 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-10-13T20:30:54Z</dc:date>
    <item>
      <title>Yocto build error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-build-error/m-p/631543#M96023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm getting error by Yocto build when local.conf adds:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;IMAGE_INSTALL_append += " vim"&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;by building it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.26.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "Debian-8.2"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6qpsabreauto"&lt;BR /&gt;DISTRO = "fsl-imx-x11"&lt;BR /&gt;DISTRO_VERSION = "3.14.52-1.1.1"&lt;BR /&gt;TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"&lt;BR /&gt;TARGET_FPU = "vfp-neon"&lt;BR /&gt;meta &lt;BR /&gt;meta-yocto = "(nobranch):b74ea963cefffad9fbd91d4eb9b240f6a8c86cd0"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia = "(nobranch):df2f700d66bace65f5d802225232d01cf511fe81"&lt;BR /&gt;meta-fsl-arm = "(nobranch):70ddee3ebeacbc53180ee7221533375bf0c9eac4"&lt;BR /&gt;meta-fsl-arm-extra = "(nobranch):41e79c6bd055f12b6252618c22c43a2fed5cfb49"&lt;BR /&gt;meta-fsl-demos = "(nobranch):17f9da65efb5c65c1d44b5cc18584034b29a742b"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk = "(nobranch):46b952b39b012cadc8a91b551ed3beee16054768"&lt;BR /&gt;meta-browser = "(nobranch):30b8d6b3d0d6501c56ef6967a2fa73a3d4bf5fe9"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-python &lt;BR /&gt;meta-ruby &lt;BR /&gt;meta-filesystems = "(nobranch):df2f700d66bace65f5d802225232d01cf511fe81"&lt;BR /&gt;meta-qt5 = "(nobranch):51b4620392aa9041d8512549bfa554bea368c5ea"&lt;/P&gt;&lt;P&gt;NOTE: Preparing RunQueue&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: No checksum specified for /mnt/work/Linux/PeterB/fsl-release-3.14.52-1.1.0_ga/downloads/vim_vim.googlecode.com_.hg._v7-4-481.tar.gz, please add at least one to the recipe:&lt;BR /&gt;SRC_URI[md5sum] = "f3c7295c7e542fba141c2f3d0ac8765c"&lt;BR /&gt;SRC_URI[sha256sum] = "0f5419388b70c62154ff3d027396b09e5acc0f028cb0ba9ce73f242d02613c39"&lt;BR /&gt;&lt;SPAN&gt;ERROR: Function failed: Fetcher failure for URL: '&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fdownloads.yoctoproject.org%2Fmirror%2Fsources%2Fvim_vim.googlecode.com_.hg._v7-4-481.tar.gz%3Bprotocol%3Dhttps%3Bmodule%3Dvim" rel="nofollow" target="_blank"&gt;http://downloads.yoctoproject.org/mirror/sources/vim_vim.googlecode.com_.hg._v7-4-481.tar.gz;protocol=https;module=vim&lt;/A&gt;&lt;SPAN&gt;'. Missing SRC_URI checksum&lt;/SPAN&gt;&lt;BR /&gt;ERROR: Logfile of failure stored in: /work/Linux/fsl-release-3.14.52-1.1.0_ga/build-x11-full/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/vim/7.4.481-r0/temp/log.do_fetch.19256&lt;BR /&gt;ERROR: Task 574 (/work/fsl-release-3.14.52-1.1.0_ga/sources/meta-openembedded/meta-oe/recipes-support/vim/vim_7.4.481.bb, do_fetch) failed with exit code '1'&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 10:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-build-error/m-p/631543#M96023</guid>
      <dc:creator>erikraynolds</dc:creator>
      <dc:date>2016-10-13T10:38:11Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto build error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-build-error/m-p/631544#M96024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erik Raynolds,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that this recipe, which is part of Open Embedded, is broken and the repository where the source was it-s no longer there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the following bug:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.yoctoproject.org/bug/bug-8253-vim-recipe-broken"&gt;https://www.yoctoproject.org/bug/bug-8253-vim-recipe-broken&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that the BSP Release you are using refers to a specific commit in the past unlike the Community BSP which is constantly changing. My recommendation would be switching to the 4.1.15 BSP Release to see if the recipe is fixed there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another alternative would be looking for the new repository for this recipe and manually fixing it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Flayers.openembedded.org%2Flayerindex%2Frecipe%2F5559%2F" rel="nofollow" target="_blank"&gt;https://layers.openembedded.org/layerindex/recipe/5559/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 20:30:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-build-error/m-p/631544#M96024</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-10-13T20:30:54Z</dc:date>
    </item>
  </channel>
</rss>