<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6UL Reference Manual - DDR density specification</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Reference-Manual-DDR-density-specification/m-p/630542#M95758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in IMX6ULRM it say in 33.1.1 , that 256Mbits-8Gbits are the supported densities of DDR devices, however 6.2 specifies a density of 256Mbytes - 4Gbytes.&lt;/P&gt;&lt;P&gt;I suppose the first one is correct and there would be no issue using a 128MByte = 1Gbit device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jan 2017 08:11:49 GMT</pubDate>
    <dc:creator>markusb</dc:creator>
    <dc:date>2017-01-19T08:11:49Z</dc:date>
    <item>
      <title>iMX6UL Reference Manual - DDR density specification</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Reference-Manual-DDR-density-specification/m-p/630542#M95758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in IMX6ULRM it say in 33.1.1 , that 256Mbits-8Gbits are the supported densities of DDR devices, however 6.2 specifies a density of 256Mbytes - 4Gbytes.&lt;/P&gt;&lt;P&gt;I suppose the first one is correct and there would be no issue using a 128MByte = 1Gbit device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 08:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Reference-Manual-DDR-density-specification/m-p/630542#M95758</guid>
      <dc:creator>markusb</dc:creator>
      <dc:date>2017-01-19T08:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL Reference Manual - DDR density specification</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Reference-Manual-DDR-density-specification/m-p/630543#M95759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; The i.MX6UL MMDC inludes the following features :&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;* x16 data bus width (2 bytes);&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;* up to 8 banks (3 bits );&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;* column size of 8–12 bits ;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;* row size of 11–16 bits.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; So, minimal address size is 8 MBytes [2 ** (11+8+3+1)] &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;and maximal one is full 4GB. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;128 MB is supported.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 04:35:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Reference-Manual-DDR-density-specification/m-p/630543#M95759</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-01-20T04:35:21Z</dc:date>
    </item>
  </channel>
</rss>