<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPerformance problems after changing the linux kernel from version 3.10.53 to 4.1.15</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Performance-problems-after-changing-the-linux-kernel-from/m-p/629138#M95521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are facing a general performance problem with kernel 4.1.15. In general the applications seem to be about 25% slower than under Kernel 3.10.53. We are using the same UBoot for both kernels with the same DDR-RAM configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone had the same problem?&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Dec 2016 15:59:04 GMT</pubDate>
    <dc:creator>trsystems</dc:creator>
    <dc:date>2016-12-20T15:59:04Z</dc:date>
    <item>
      <title>Performance problems after changing the linux kernel from version 3.10.53 to 4.1.15</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-problems-after-changing-the-linux-kernel-from/m-p/629138#M95521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are facing a general performance problem with kernel 4.1.15. In general the applications seem to be about 25% slower than under Kernel 3.10.53. We are using the same UBoot for both kernels with the same DDR-RAM configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone had the same problem?&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2016 15:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-problems-after-changing-the-linux-kernel-from/m-p/629138#M95521</guid>
      <dc:creator>trsystems</dc:creator>
      <dc:date>2016-12-20T15:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: Performance problems after changing the linux kernel from version 3.10.53 to 4.1.15</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-problems-after-changing-the-linux-kernel-from/m-p/629139#M95522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oliver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check as possible reason&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/371109"&gt;Cortex-A9 ARM Errata 845369&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can try with nxp official bsps from link below, they use kernel 3.10.53 with&lt;/P&gt;&lt;P&gt;uboot v2014.04 and kernel 4.1.15 with uboot v2015.04&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW"&gt;i.MX 6 Series Software and Development Tool|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2016 08:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-problems-after-changing-the-linux-kernel-from/m-p/629139#M95522</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-21T08:04:07Z</dc:date>
    </item>
  </channel>
</rss>