<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Use IPU2 CSI1 for adv7180 camera fail</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Use-IPU2-CSI1-for-adv7180-camera-fail/m-p/628994#M95497</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi wilson&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for adv7180 mxc_v4l2_tvin.out should be used, also seems&lt;/P&gt;&lt;P&gt;this configuration is used on BD board imx6q-nitrogen6x.dts&lt;BR /&gt;&lt;A href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6x.dts"&gt;https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6x.dts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jan 2017 06:53:10 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-19T06:53:10Z</dc:date>
    <item>
      <title>Use IPU2 CSI1 for adv7180 camera fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-IPU2-CSI1-for-adv7180-camera-fail/m-p/628993#M95496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I want to use the ipu2 csi1 for adv7180 camera,but i fail.&lt;/P&gt;&lt;P&gt;I have use the tips :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-158531"&gt;iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and the boundarydevice's kernel.&lt;/P&gt;&lt;P&gt;the adv7180 driver is ok,but when i open the camera app,it send:&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: mxc_v4l2_prepare_bufs buffers not allocated,index=0, length=622080&lt;BR /&gt;ERROR: v4l2 capture: mxc_streamon buffer has not been queued yet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the OS is the android4.4.2 android android5.1.1, the errors is the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what's the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 03:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-IPU2-CSI1-for-adv7180-camera-fail/m-p/628993#M95496</guid>
      <dc:creator>wilsonchen</dc:creator>
      <dc:date>2017-01-19T03:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: Use IPU2 CSI1 for adv7180 camera fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-IPU2-CSI1-for-adv7180-camera-fail/m-p/628994#M95497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi wilson&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for adv7180 mxc_v4l2_tvin.out should be used, also seems&lt;/P&gt;&lt;P&gt;this configuration is used on BD board imx6q-nitrogen6x.dts&lt;BR /&gt;&lt;A href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6x.dts"&gt;https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts/imx6q-nitrogen6x.dts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 06:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-IPU2-CSI1-for-adv7180-camera-fail/m-p/628994#M95497</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-19T06:53:10Z</dc:date>
    </item>
  </channel>
</rss>