<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: u-boot porting fail</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-fail/m-p/628277#M95379</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Coiln&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for enabling i.MX6Solo one can look at sect.5 Enabling Solo Emulation&lt;/P&gt;&lt;P&gt;attached Linux Guide. From log seems there problems with i2c communication&lt;/P&gt;&lt;P&gt;with pmic, one can check i2c signals with oscilloscope, use jtag for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jan 2017 23:43:39 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-19T23:43:39Z</dc:date>
    <item>
      <title>u-boot porting fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-fail/m-p/628276#M95378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While porting u-boot(2016.03-r0), the below debug message appeared on the console.&lt;/P&gt;&lt;P&gt;How to fix this error at the first...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:21:13 -05 00)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6SOLO rev1.3 996 MHz (running at 792 MHz)&lt;BR /&gt;CPU: Extended Commercial temperature grade (-20C to 105C) at 51C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;force_idle_bus: sda=1 scl=0 sda.gp=0x6d scl.gp=0x6c&lt;BR /&gt;force_idle_bus: failed to clear bus, sda=1 scl=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=1&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x21a4000&lt;BR /&gt;Can't find PMIC:PFUZE100&lt;BR /&gt;initcall sequence 4ff968f0 failed at call 178040a4 (err=-19)&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 08:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-fail/m-p/628276#M95378</guid>
      <dc:creator>coilnpark</dc:creator>
      <dc:date>2017-01-19T08:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot porting fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-fail/m-p/628277#M95379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Coiln&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for enabling i.MX6Solo one can look at sect.5 Enabling Solo Emulation&lt;/P&gt;&lt;P&gt;attached Linux Guide. From log seems there problems with i2c communication&lt;/P&gt;&lt;P&gt;with pmic, one can check i2c signals with oscilloscope, use jtag for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 23:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-fail/m-p/628277#M95379</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-19T23:43:39Z</dc:date>
    </item>
  </channel>
</rss>