<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NAND Flash on iMX53 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190565#M9532</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;is there anybody who has a desin example from a NAND flash connected to the iMX537 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Nov 2011 13:31:36 GMT</pubDate>
    <dc:creator>jomeke</dc:creator>
    <dc:date>2011-11-24T13:31:36Z</dc:date>
    <item>
      <title>NAND Flash on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190565#M9532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;is there anybody who has a desin example from a NAND flash connected to the iMX537 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2011 13:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190565#M9532</guid>
      <dc:creator>jomeke</dc:creator>
      <dc:date>2011-11-24T13:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190566#M9533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The connection is quite straight. You can use the reference manual of the i.MX53 / table 5-3 at section 5.3.4.&lt;/P&gt;&lt;P&gt;You'll find there that the NAND control signals are dedicated pins with the same name.&lt;/P&gt;&lt;P&gt;Nevertheless, the data bus is not dedicated, and can be used on the PATA signals or EIM data signals.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At boot, it is important to let the processor knows where to use the data bus, and the table 7-14 at section 7.5.2.4 explains this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can check that board for a reference:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2011 17:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190566#M9533</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2011-11-24T17:21:00Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190567#M9534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the information Florent&lt;BR /&gt; &lt;BR /&gt;&lt;CITE&gt;Florent Auger said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/nand-flash-on-imx53?groupUrl=imx53quickstartboard&amp;amp;commentId=4103961%3AComment%3A46755&amp;amp;xg_source=msg_com_gr_forum#4103961Comment46755"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The connection is quite straight. You can use the reference manual of the i.MX53 / table 5-3 at section 5.3.4.&lt;/P&gt;&lt;P&gt;You'll find there that the NAND control signals are dedicated pins with the same name.&lt;/P&gt;&lt;P&gt;Nevertheless, the data bus is not dedicated, and can be used on the PATA signals or EIM data signals.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At boot, it is important to let the processor knows where to use the data bus, and the table 7-14 at section 7.5.2.4 explains this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can check that board for a reference:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIM...&lt;/A&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2011 07:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190567#M9534</guid>
      <dc:creator>jomeke</dc:creator>
      <dc:date>2011-11-25T07:13:20Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190568#M9535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am porting u-boot for an mx53 board which has 512 MB Nand flash of Samsung K9F4G08.&lt;/P&gt;&lt;P&gt;It uses CS0 and 8 bit interface only. So which value should be for CONFIG_SYS_NAND_BASE? &lt;/P&gt;&lt;P&gt;The connection signal is below:&lt;/P&gt;&lt;P&gt;- NANDF_CS0&amp;nbsp; --&amp;gt; CS (to NAND chip)&lt;/P&gt;&lt;P&gt;- NANDF_CS1,2,3 --&amp;gt; not used&lt;/P&gt;&lt;P&gt;- PATA_DATA[0-7] --&amp;gt; DATA[0-7]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Expecting your help!!&lt;/P&gt;&lt;P&gt;HTH&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2012 03:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-on-iMX53/m-p/190568#M9535</guid>
      <dc:creator>hoanghoa</dc:creator>
      <dc:date>2012-11-30T03:16:24Z</dc:date>
    </item>
  </channel>
</rss>