<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re:  Are the Bit Positions on FTM module correct in reference manual { REV : 0.1 }</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627898#M95281</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Arter, this is very helpful&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 09:12:43 GMT</pubDate>
    <dc:creator>liamd</dc:creator>
    <dc:date>2016-09-22T09:12:43Z</dc:date>
    <item>
      <title>Are the Bit Positions on FTM module correct in reference manual { REV : 0.1 }</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627896#M95279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The bit positions in Reference manual 0.1 seem to be in the incorrect position can I get clarifications about this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; background-color: #ffffff; font-size: 14px;"&gt;Looking at the reference manual { 0.1, 08/2016 }, FTM registers are bit number [ 0:31 ] where the GPT registers are numbered [ 31:0 ]. for example is WPDIS in bit position 29 or bit position 3 ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; background-color: #ffffff; font-size: 14px;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 09:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627896#M95279</guid>
      <dc:creator>liamd</dc:creator>
      <dc:date>2016-09-19T09:46:08Z</dc:date>
    </item>
    <item>
      <title>Re:  Are the Bit Positions on FTM module correct in reference manual { REV : 0.1 }</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627897#M95280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean the Reference Manual document for the i.MX7Dual processor? If so, this is just the typo in the manual. The bit numbering order, shown in the FTM chapter, is wrong. The bits should be numbered [31:0], as usual. For the correct bit numbering, please refer to the FlexTimer module chapter in the Vybrid series Reference Manual document (the Vybrid series processors use the same FlexTimer module as i.MX7Dual/Solo), available on the Vybrid Documentation web page:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Fvfxxx-controller%2Ff-series%2Farm-cortex-a5-plus-cortex-m4-mpus-1.5-mb-sram-lcd-security-ethernet-l2-switch%3AVF6xx%3Ffpsp%3D1%26tab%3DDocumentation_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/vfxxx-controller/f-series/arm-cortex-a5-plus-cortex-m4-mpus-1.5-mb-sram-lcd-security-ethernet-l2-switch:VF6xx?fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 09:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627897#M95280</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-09-21T09:26:58Z</dc:date>
    </item>
    <item>
      <title>Re:  Are the Bit Positions on FTM module correct in reference manual { REV : 0.1 }</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627898#M95281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Arter, this is very helpful&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 09:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Are-the-Bit-Positions-on-FTM-module-correct-in-reference-manual/m-p/627898#M95281</guid>
      <dc:creator>liamd</dc:creator>
      <dc:date>2016-09-22T09:12:43Z</dc:date>
    </item>
  </channel>
</rss>