<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6 ipu CSI examples</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ipu-CSI-examples/m-p/627092#M95191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am using i.MX6 with 3.14.60-fslc-imx6-sr linux kernel&lt;/P&gt;&lt;P&gt;I am trying to use IPU to capture parallel 8bit camera frames.&lt;/P&gt;&lt;P&gt;I have read examples available on &lt;A class="link-titled" href="https://github.com/rogeriorps/ipu-examples/tree/master/mx6" title="https://github.com/rogeriorps/ipu-examples/tree/master/mx6"&gt;ipu-examples/mx6 at master · rogeriorps/ipu-examples · GitHub&lt;/A&gt;&amp;nbsp; and have seen that &lt;BR /&gt;#include&amp;lt;linux/ipu-v3.h&amp;gt; header has got functions with CSI but it doesn't compile. Headers that compile are &amp;lt;linux/mxcfb.h&amp;gt; and &amp;lt;linux/ipu.h&amp;gt; But with them I have completly got NO IDEA how to set CSI to be input for IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also saw that IPUlib doesnt work in imx6 but only with imx53 so I think that is the reason why &amp;lt;linux/ipu-v3.h&amp;gt; header doesn't compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me which headers should I use or give some example codes in c++ of setting CSI as an input for IPU ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Nov 2016 13:18:44 GMT</pubDate>
    <dc:creator>sebaseba</dc:creator>
    <dc:date>2016-11-28T13:18:44Z</dc:date>
    <item>
      <title>i.MX6 ipu CSI examples</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ipu-CSI-examples/m-p/627092#M95191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am using i.MX6 with 3.14.60-fslc-imx6-sr linux kernel&lt;/P&gt;&lt;P&gt;I am trying to use IPU to capture parallel 8bit camera frames.&lt;/P&gt;&lt;P&gt;I have read examples available on &lt;A class="link-titled" href="https://github.com/rogeriorps/ipu-examples/tree/master/mx6" title="https://github.com/rogeriorps/ipu-examples/tree/master/mx6"&gt;ipu-examples/mx6 at master · rogeriorps/ipu-examples · GitHub&lt;/A&gt;&amp;nbsp; and have seen that &lt;BR /&gt;#include&amp;lt;linux/ipu-v3.h&amp;gt; header has got functions with CSI but it doesn't compile. Headers that compile are &amp;lt;linux/mxcfb.h&amp;gt; and &amp;lt;linux/ipu.h&amp;gt; But with them I have completly got NO IDEA how to set CSI to be input for IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also saw that IPUlib doesnt work in imx6 but only with imx53 so I think that is the reason why &amp;lt;linux/ipu-v3.h&amp;gt; header doesn't compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me which headers should I use or give some example codes in c++ of setting CSI as an input for IPU ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 13:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ipu-CSI-examples/m-p/627092#M95191</guid>
      <dc:creator>sebaseba</dc:creator>
      <dc:date>2016-11-28T13:18:44Z</dc:date>
    </item>
  </channel>
</rss>